Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General MicroZed power, USB and backplane?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 371 subscribers
  • Views 1132 views
  • Users 0 members are here
Related

MicroZed power, USB and backplane?

rdb98789
rdb98789 over 2 years ago

Hello, we have created a MicroZed carrier card that provides the 5V power source through the expansion connectors. However, we like to plug in the USB cable sometimes to see the serial printout. Some questions:

1) Is there any issue in having both supplies connected at once? So USB cable connected as well as the 5V regulator on our carrier card?

2) Is there any way to disable getting powered via USB? I'd like to test some power cycle reboot stuff while watching the USB UART data, but I need a true power cycle (including the carrier card components which is not powered by USB). Any recommendations?

  • Sign in to reply
  • Cancel

Top Replies

  • felixholzman
    felixholzman over 2 years ago +1
    Hallo, danke für Ihre Fragen bezüglich des MicroZed-Boards und der Stromversorgung über USB . Hier sind einige Antworten auf Ihre Fragen: Es sollte keine Probleme geben, wenn sowohl die USB-Verbindung…
Parents
  • rdb98789
    0 rdb98789 over 2 years ago

    I do see now in the Microzed schematic notes they have a "USB Self powered, no backfeed" option, but requires some hardware mods. So JT7 pins 2-3 gets a zero ohm resistor as opposed to the default 2-1, populate D10 and D11, do not populate R97 and R98. But you're saying that even with that, the Microzed would still power up and boot via USB power because D4 is installed? So do all of the above, plus remove D4, and now it's only able to be powered from the VIN_HDR, and USB-UART will still function?

    Or could I do all the above, skip D4 removing D4, but instead cut the 5V wire out of the USB cable?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • padudle
    0 padudle over 2 years ago in reply to rdb98789

    I think you want to keep the usb-uart chip powered by VBUS on the usb cable. Othewise, you have to reconnect the serial termal application after every power cycle and you cannot see what happens at power up time.

    As I read the schematic, removing D4 is the only way to isolate VBUS from VIN.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • padudle
    0 padudle over 2 years ago in reply to rdb98789

    I think you want to keep the usb-uart chip powered by VBUS on the usb cable. Othewise, you have to reconnect the serial termal application after every power cycle and you cannot see what happens at power up time.

    As I read the schematic, removing D4 is the only way to isolate VBUS from VIN.