Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
i.MX 8M+ Edge AI Kit Access to i210 on SMARC SOM?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 366 subscribers
  • Views 1138 views
  • Users 0 members are here
Related

Access to i210 on SMARC SOM?

andynic
andynic over 2 years ago

Hi, 

I'm trying to figure out if the IMX8M Plus Edge AI kit allows access to the Intel i210 which is, evidently on the SMARC SOM? Is the diagram below from AVNET correct -- it shows 2 PHYs connected to the same network box which seems wrong?

Highlighted box below.

image

Is the i210 on the Carrier board or on the IMX8M SOM?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 2 years ago

    Hi,

    That diagram looks faulty. The one below from the PDF hardware manual looks corrected, showing what the interface is to the i210 on the carrier board, with no weird connections like the earlier diagram! : ) 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andynic
    0 andynic over 2 years ago in reply to shabaz

    That is fantastic. Just awesome because I was hoping to find a PCBA where an i210 and DP83867 were simultaneously connected. I thought I was going to need to build a custom PCBA, but now I can use this one. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • andynic
    0 andynic over 2 years ago in reply to shabaz

    That is fantastic. Just awesome because I was hoping to find a PCBA where an i210 and DP83867 were simultaneously connected. I thought I was going to need to build a custom PCBA, but now I can use this one. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • peterfenn
    0 peterfenn over 2 years ago in reply to andynic

    The first block diagram (from the Product Brief) incorrectly shows both the assembly options available on the Carrier Board for the second Ethernet port. The second diagram (from Hardware User’s Guide) correctly describes the implementation of second Ethernet port in this 8Mplus Edge AI Kit.