Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design Testing and getting wrong data from SPI BUS on Maaxboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 1104 views
  • Users 0 members are here
  • yocto image build
  • Maaxboard RT
  • spi
  • maaxboard
  • dts
Related

Testing and getting wrong data from SPI BUS on Maaxboard

zafersen
zafersen over 4 years ago

Hi,

I am working on spi bus on maaxboard's j10 expansion pin. According to the MaaXBoard-Hardware_UserManual-V1.2-EN.pdf, 19-21-23-24th pins on it are ecspi1 outputs. When I write data over spi, I can get correct data from the mosi line but the miso and cs lines are completely inaccurate. Something might be wrong with the document or there might be another device on the line. So I edited the device tree file and the problem with the cs line was solved by when I changed the cs pinout. I am going to share some pictures which indicate data on ecspi1

if possible, could you please tell me where to download the schematics for Maaxboard?

 

Thanks in Advance!!

ecspi pinout configuration in dts:

&ecspi1{
	fsl,spi-num-chipselects = < 1 >;
	cs-gpios = <&gpio5 13 1 >, <&gpio3 2 1 >;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_ecspi1 >;
	status = "okay";
	#address-cells=<1>;
	#size-cells=<0>;
	spidev@0x00{
		#address-cellss=<1>;
		#size-cells=<0>;
		compatible = "spidev", "semtech,sx1301";
		spi-max-frequency = <1000000>;
		reg = <0>;
	};
	anotherspidev@0x00 {
		//status = "disabled";
		compatible = "spidev", "semtech,sx1301";
		spi-max-frequency = <400000>;
		reg = <1>;
	};
};

the first image is when I use gpio5 13(default) as the cs pin 

the second image is when I use a different pin (gpio3 2) as the cs pin. 

d1=> MISO

d2=> MOSI

d3=> CS

d4=> CLK

pic-2

pic-3

  • Sign in to reply
  • Cancel
  • jafoste4
    jafoste4 over 4 years ago

    Hello Zafersen,

    Please reach out to your local Avnet FAE whom can request them upon your behalf.

    Thank you,

    Josh