• Products and Partners
    Products and Partners
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
Avnet Boards Forums
  • Products and Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design MaaXBoard-RT: PinMux, 2nd SPI, other features
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 1306 views
  • Users 0 members are here
  • peripherals
  • pins
  • header
  • MaaXBoard-RT
  • Maaxboard RT
  • signals
  • alternatives
  • Pin Mux
Related

MaaXBoard-RT: PinMux, 2nd SPI, other features

tjaekel
tjaekel over 3 years ago

I was checking the headers J1 and J15, if I could have a 2nd SPI:
I want to implement "my" DualSPIder approach: one SPI master Tx, one SPI slave RX.
So, I have checked the header signals, pins and possible alternatives.

image

Figure 1: The AVNET J1 pin table (with corrections)

PinMux_Alternatives

Figure 2: The pin names and possible (potential, not all) alternatives for the signals:
bold and green - what is configured on my project

QUESTION:
What is this GPIO2_IO15 as "GPIO/CTS"?
There is not a GPIO2 (just a GPIO_MUX2_IO15) and LPUART1_CTS is on a different pin.

What are the default features (signals)?

  • 2x I2C
  • 2x UART
  • 1s SPI
  • 1x SAI, bi-directional (but just as SAI Master)

plus on J15:

  • 1x CAN
  • 1x I2C

I have not listed here PWMs or ADC signals.

How to have a 2nd SPI?

A second SPI is possible, if you use the pins for LPUART1.
This is actually the Debug UART (the 3-pin header for the MCU-LINK).
But you can make it free and route the Debug UART, e.g. as LPUART6 (or even LPUART2 possible),
just change FW and connect MCU-LINK on other pins, to make LPUART1 free (as 2nd SPI).

So, a second SPI is available if you use another Debug UART.

What other features would be possible?

Based on the Alternatives for the pins - here what else could be configured and be available:

  • SAI3_MCLK : the master clock for PCM (if needed):
    BUT! the SAI3_RX_SYNC is not available. So, you can run the PCM as bi-directional) but just as Master.
    A PCM Slave is not possible!
  • SPDIF_OUT
  • SPDIF_IN
  • PDM with PDM_CLK and PDM_DATA0 (e.g. for an external PDM MIC) (on J15)
  • maybe two additional CAN (on J15)
  • or, maybe, another UART (on J15)
  • some more PWMs
  • Sign in to reply
  • Cancel
Parents
  • tjaekel
    tjaekel over 2 years ago

    Here the final pinmux table I want to use...
    Bear in mind: I have verified the pin functions (before I would start my own PCB design...).
    e.g. pin J1, p36, is "GPIO8_IO15" or "GPIO_MUX2_IO15" --> as CM7_GPIO2...

    Maaxboard-RT-pinmux

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tjaekel
    tjaekel over 2 years ago

    Here the final pinmux table I want to use...
    Bear in mind: I have verified the pin functions (before I would start my own PCB design...).
    e.g. pin J1, p36, is "GPIO8_IO15" or "GPIO_MUX2_IO15" --> as CM7_GPIO2...

    Maaxboard-RT-pinmux