Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Xilinx XADC
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 362 subscribers
  • Views 3276 views
  • Users 0 members are here
Related

Xilinx XADC

e14 Contributor
e14 Contributor over 13 years ago

Is there a reason you didn't include the A/D convertors in the expansion headers?  Having these are very useful.

  • Sign in to reply
  • Cancel
Parents
  • nitron
    0 nitron over 13 years ago

    I couldn't agree more with the previous post!
    One of the differentiating features of the Zynq 7000 is the integrated ADC (in fact 2 ADC 1Msamples/s each). You do not find them on Altera's Cyclone V!
    Is there any hope to be able to use them in next versions?
    Is there any (equivalent) substitute available ?

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to nitron

    An XADC Header is provided in the new I/O Carrier Card.  Documentation for that has recently been posted on the site.  I agree that the AMS/XADC feature of Zynq sets it apart from the competing Altera solutions.  What applications are you using in for - voltage monitoring, temperature monitoring, etc.?

    Would it be helpful if Avnet came out with more reference designs focusing in on XADC?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to nitron

    An XADC Header is provided in the new I/O Carrier Card.  Documentation for that has recently been posted on the site.  I agree that the AMS/XADC feature of Zynq sets it apart from the competing Altera solutions.  What applications are you using in for - voltage monitoring, temperature monitoring, etc.?

    Would it be helpful if Avnet came out with more reference designs focusing in on XADC?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • nitron
    0 nitron over 13 years ago in reply to e14 Contributor

      Looking at the I/O Carrier Card schematics (rev D.preliminary) it appears that it has only two differential analog inputs...

      In a "real life" application, for instance for motor control, up to 16 channels are used to measure phase currents, phase voltages, temperatures, etc.

       The two ADCs are started simultaneously by a timer underflow and overflow.
       The timer has a frequency between 4 and 100kHz. This makes a sampling frequency between 8 and 200kHz.
       Each ADC converts 8 channel (16 in total). At the end of conversion an interrupt is generated and the conversion results are treated by software (fast loop running at 8-200kHz).
       The timer is usually a PWM (Pulse Width Modulation) timer. It allows the synchronisation of PWM pulses (converter command) with the A/D conversions.

    A reference design showing how to instantiate the XADC (the 16 auxiliary analogue channels), to start A/D sequences from a timer underflow/overflow and to generate PWM pulses will be greatly appreciated!

    Are all the 16 auxiliary analogue XADC channels accessible at the MicroZed connectors ?(not the I/O Carrier card but the MicroZed)

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi

    I use the zed board for the main I/O for robots.  So having a ADC is very useful.  Not sure how many you would really need to pin out on the micro, but I would say 8 would be a good number.

    Thanks

    bren

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    P.S

    i should add we make our own carrier boards.  So just need the XADC in the main header.

    Thanks

    Bren