Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Write data in DDR3 through PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 597 views
  • Users 0 members are here
Related

Write data in DDR3 through PL

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone,

I have developed a vhdl file that writes data inside the DDR3. I don't have the AXI BFM licence so I simulated my AXI interface with a BRAM controller that provides an AXI slave interface and it works.

Then I connect my design to AXI HP0 of the Processing system (I delete previous BRAM controller). My problem is that no data is written inside the DDR3 when I verify it by doing a memory dump with SDK.

Do anyone have idea or a reference design or a guide or a source code that works to write data burst correctly inside the DDR3 through the PL?

Thank you

Ny

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The AXI HP interfaces operate with the PL Logic as a Master and the PS interface as the Slave interface as opposed to the way your AXI Slave BRAM controller works. If this is what you want to implement you can take a look at this Xilinx AR for an example: http://www.xilinx.com/support/answers/54274.htm

     

    If you want to implement logic in the PL that operates as an AXI Slave, in a similar fashion to the BRAM controller, the labs for the current Avnet Zynq HW Speedway provide an example of implementing DMA transfers from a BRAM AXI Slave in the PL to the DDR memory. If you are unable to attend the Speedway in person check with your Avnet/Silica FAE for the course materials.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The AXI HP interfaces operate with the PL Logic as a Master and the PS interface as the Slave interface as opposed to the way your AXI Slave BRAM controller works. If this is what you want to implement you can take a look at this Xilinx AR for an example: http://www.xilinx.com/support/answers/54274.htm

     

    If you want to implement logic in the PL that operates as an AXI Slave, in a similar fashion to the BRAM controller, the labs for the current Avnet Zynq HW Speedway provide an example of implementing DMA transfers from a BRAM AXI Slave in the PL to the DDR memory. If you are unable to attend the Speedway in person check with your Avnet/Silica FAE for the course materials.

     

    -Gary