Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Net lengths and clocking pins
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 422 views
  • Users 0 members are here
Related

Net lengths and clocking pins

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I am designing a carrier board for microzed that will interface an ADC. It has an 8 wire LVDS interface and timing is quite critical.

I am trying to confirm which pins on the JX headers correspond to the MRCC and SRCC capable pairs. The pinout in the Altium librtary does not explicitly specify...

I have found the spreadsheet with the net lengths which is great, but can I confirm that for example:

JX1_LVDS_11_P connects to IO_L11P_T1_SRCC_35 on the chip.

Many thanks in advance!

Ben.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Actually JX1_LVDS_11_P is connected to IO_L12P_T1_MRCC_34 (Zynq package pin U18).

    ( I know, the MicroZed JX LVDS pair numbers do not match up with the Xilinx signal pair number names ).

     

    You can verify this using the MicroZed Schematic and/or the MicroZed Master XDC file (generated from the netlist), both found here:

     

    http://zedboard.org/support/documentation/1519

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Actually JX1_LVDS_11_P is connected to IO_L12P_T1_MRCC_34 (Zynq package pin U18).

    ( I know, the MicroZed JX LVDS pair numbers do not match up with the Xilinx signal pair number names ).

     

    You can verify this using the MicroZed Schematic and/or the MicroZed Master XDC file (generated from the netlist), both found here:

     

    http://zedboard.org/support/documentation/1519

     

    -Gary