Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design FPGA fabric clock input?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 484 views
  • Users 0 members are here
Related

FPGA fabric clock input?

e14 Contributor
e14 Contributor over 13 years ago

I can't seem to find an external clock to the FPGA fabric on the MicroZed. Does it have to get the clock from the processor subsystem or from one of the microheaders?

  • Sign in to reply
  • Cancel
Parents
  • rwong1231
    0 rwong1231 over 9 years ago

    Hi,

    With respect to the information above, then would the following be valid:

    I have a 80 MSPS 16-bit TI ADC board (via FMC).

    I'm planning on getting the MicroZed Z7020 (where the PS is clocked at 667 MHz).

    Thus:

    using two-wire (LVDS) approach - (16bit x 80 MSPS)/2 = 640 MHz required bit clock rate for the ADC.

    Would my MicroZed be capable of handling the capture since its 667 MHz?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rwong1231
    0 rwong1231 over 9 years ago

    Hi,

    With respect to the information above, then would the following be valid:

    I have a 80 MSPS 16-bit TI ADC board (via FMC).

    I'm planning on getting the MicroZed Z7020 (where the PS is clocked at 667 MHz).

    Thus:

    using two-wire (LVDS) approach - (16bit x 80 MSPS)/2 = 640 MHz required bit clock rate for the ADC.

    Would my MicroZed be capable of handling the capture since its 667 MHz?