Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design FPGA fabric clock input?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 482 views
  • Users 0 members are here
Related

FPGA fabric clock input?

e14 Contributor
e14 Contributor over 13 years ago

I can't seem to find an external clock to the FPGA fabric on the MicroZed. Does it have to get the clock from the processor subsystem or from one of the microheaders?

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Nocturnalpea,

    You should look into using the SERDES IP block(SelectIO Interface Wizard). This IP block is used for LVDS to bring the data into the fabric serial and convert it to a slower more manageable clock with the data in parallel. This inturn limits the HIGH speed to as few logic cells as possible which helps your timing. That is if you really do need the 640MHz, if you pass into the SERDES IP block you will only need a 40MHz clock to perform operations on the data.

    Another thing to note is depending on the pins used you may only hit 600Mb/s (LVDS) per lane.

    https://www.xilinx.com/support/documentation/data_sheets/ds181_Artix_7_Data_Sheet.pdf

    So as for your question of will it work. It depends. It turns into a question of will it work how you intend it to. Maybe, but if you use the SERDES IP block, then most likely yes.

    I am going to suggest that you ask any further questions in relationship to getting your TI FMC working over at the TI Forum as they will have more experience in implementing their own boards.

    https://e2e.ti.com/support/

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Nocturnalpea,

    You should look into using the SERDES IP block(SelectIO Interface Wizard). This IP block is used for LVDS to bring the data into the fabric serial and convert it to a slower more manageable clock with the data in parallel. This inturn limits the HIGH speed to as few logic cells as possible which helps your timing. That is if you really do need the 640MHz, if you pass into the SERDES IP block you will only need a 40MHz clock to perform operations on the data.

    Another thing to note is depending on the pins used you may only hit 600Mb/s (LVDS) per lane.

    https://www.xilinx.com/support/documentation/data_sheets/ds181_Artix_7_Data_Sheet.pdf

    So as for your question of will it work. It depends. It turns into a question of will it work how you intend it to. Maybe, but if you use the SERDES IP block, then most likely yes.

    I am going to suggest that you ask any further questions in relationship to getting your TI FMC working over at the TI Forum as they will have more experience in implementing their own boards.

    https://e2e.ti.com/support/

    --Josh