Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Question Regarding MicroZED
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 667 views
  • Users 0 members are here
Related

Question Regarding MicroZED

e14 Contributor
e14 Contributor over 12 years ago

Hi,
I looked at MicroZED and it looks like a very nice piece of hardware for beginners.

Well, But, I have a question regarding this board.

What is the programming interface of this board? Is it PC4?

In ZEDBoard, or ZC-702 or ... the interface is USB, thanks to the Digilent USB JTAG interface.

Now, for MicroZED, PC4????
Do you mean one needs a computer with Parallel port to program the board? Isn't that a little bit silly?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 12 years ago

    You are correct that MicroZed does not have on-board USB-JTAG circuitry. The reference to the PC4 is a reference to the 2x7 socket only, which is on the MicroZed and attached to the PL JTAG pins of the Zynq. We obviously don't expect people to use an old parallel JTAG cable. The Xilinx Platform Cable uses the same PC4 connection. The Digilent HS1 or HS2 also ship with an adapter that fits the PC4 socket. Since the Digilent HS1 and HS2 are faster and 1/4th the cost of the Xilinx cable, those are what we recommend. Avnet sells these cables along with a flex cable (AES-ACC-XP4-HS2) replacement for the rigid PC4 adapter.

    http://em.avnet.com/jtaghs2

    http://www.em.avnet.com/en-us/design/drc/Pages/Digilent-JTAG-HS1-Programming-Cable.aspx

    http://avnetexpress.avnet.com/store/em/EMController/Development-Kits/Avnet-Design-Services-Custom/AES-ACC-XP4-HS2/_/R-5004400969587/A-5004400969587/An-0?action=part&catalogId=500201&langId=-1&storeId=500201&listIndex=-1&page=1&rank=1

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 12 years ago

    You are correct that MicroZed does not have on-board USB-JTAG circuitry. The reference to the PC4 is a reference to the 2x7 socket only, which is on the MicroZed and attached to the PL JTAG pins of the Zynq. We obviously don't expect people to use an old parallel JTAG cable. The Xilinx Platform Cable uses the same PC4 connection. The Digilent HS1 or HS2 also ship with an adapter that fits the PC4 socket. Since the Digilent HS1 and HS2 are faster and 1/4th the cost of the Xilinx cable, those are what we recommend. Avnet sells these cables along with a flex cable (AES-ACC-XP4-HS2) replacement for the rigid PC4 adapter.

    http://em.avnet.com/jtaghs2

    http://www.em.avnet.com/en-us/design/drc/Pages/Digilent-JTAG-HS1-Programming-Cable.aspx

    http://avnetexpress.avnet.com/store/em/EMController/Development-Kits/Avnet-Design-Services-Custom/AES-ACC-XP4-HS2/_/R-5004400969587/A-5004400969587/An-0?action=part&catalogId=500201&langId=-1&storeId=500201&listIndex=-1&page=1&rank=1

     

    Bryan