Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design DDR Configuration
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 1289 views
  • Users 0 members are here
Related

DDR Configuration

e14 Contributor
e14 Contributor over 13 years ago

I need help configuring the memory interfaces in XPS.  I'm trying to follow the Speedway tutorial.  The ZedBoard hardware user guide specifies all the calculation results for configuring the DDR timing, but the Micro Zed doesn't have the same level of details.


I was trying to recreate Zed Board calculations (I can't find a link to the worksheet for this that Xilinx provided), and I think I was successful.  I then tried to apply the calculations to the MicroZed net lengths.


It sounds like the Zed Board only had one memory chip, while the Micro Zed has 2.  I didn't know how to compensate for that either.



I can't find the  two Micron MT41K256M16HA-125:E DDR3 memory part in the tool either.


My work so far if that helps.  I combined the Net length lists for Zed Board and Micro Zed in the same spread sheet.



https://docs.google.com/spreadsheet/ccc?key=0Ao_cHWinWfHUdER5TDMyai11eC1JUk9FcFcyUkRsVXc&usp=sharing



(not publicly editable, but commenting should be allowed)

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    We learned a lot when we designed ZedBoard, and we went to a lot more effort with MicroZed in relation to the DDR3 layout. Xilinx specifies that internal package delays should be included in the trace length matching calculations. This was not done on ZedBoard. On MicroZed, we routed and matched trace lengths to be inclusive of the internal package delay on the Zynq.

     

    You also asked what you do when there are two chips. Both ZedBoard and MicroZed have two DDR3 chips, each of which is 16-bits wide. If fly-by (daisy-chain) routing is used, then you use the mid-point between the two chips.

     

    We have pre-calculated these values for you and included them in a new Preset file that is available on the MicroZed Documentation page. You will also find 3 new tutorials posted this morning that will get you started. These tutorials will walk you through the process of using Vivado 2013.2 to create a new Zynq Hardware platform (including using the Preset file to pull in the MicroZed specific settings) and then SDK to create and run applications on MicroZed.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bhfletcher

    Thanks for the quick response.  I was able to use the Vivado tutorial for Micro Zed and the Speedway Lab 8 Into To Zynq for Zed Board to create a micro SD boot.bin Hello World application.

    I've also run into this issue:
    http://www.xilinx.com/support/answers/56819.htm

    I'm not able to reconfigure the IP for the Zynq in Vivado on 64-bit Linux (Specifically Ubuntu 12.04 LTS).  Haven't had a chance to try the patch myself, but will later tonight.  Thought I would point it out as a potential pitfall to other folks using Vivado for Micro Zed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bhfletcher

    Thanks for the quick response.  I was able to use the Vivado tutorial for Micro Zed and the Speedway Lab 8 Into To Zynq for Zed Board to create a micro SD boot.bin Hello World application.

    I've also run into this issue:
    http://www.xilinx.com/support/answers/56819.htm

    I'm not able to reconfigure the IP for the Zynq in Vivado on 64-bit Linux (Specifically Ubuntu 12.04 LTS).  Haven't had a chance to try the patch myself, but will later tonight.  Thought I would point it out as a potential pitfall to other folks using Vivado for Micro Zed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bhfletcher
    0 bhfletcher over 13 years ago in reply to e14 Contributor

    Thanks for sharing the link for this patch. I will re-post in the tools Forum as well.

    Bryan