Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed PS + PL with vivado 2013.4 and Linux command
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 361 subscribers
  • Views 1010 views
  • Users 0 members are here
Related

MicroZed PS + PL with vivado 2013.4 and Linux command

e14 Contributor
e14 Contributor over 12 years ago

Hi everybody.

I'm novice with ZYNQ SoC design. I bought a MicroZed board and I ran  01_MicroZed_Zynq_Intro_2013_2_01.pdf and Micro_zed_getting_started_v1.1.pdf tutorials. Everything was good (clear and simple).

Now I would like to generate a bitstream with PS + PL under Vivado
The idea is to implement a simple R/W register (32 bits) into PL. I would like to perform read/write on this register thanks to Linux command. Thus. I will be sure that PL is well configured.


Could you help me to do that ?
Which tools do I have to use ?
How to implement the register into PL into the Vivado project
How to connect PS to this register ?
Do I need any Linux driver to accees to the register via TeraTerm?


I know I have to convert bitstream.bit into bitstream.bit.bin as explained into xilinx AR# 46913 but I don't manage to do it.


I find this tuto MicroZed_Open_Source_Linux_In_System_QSPI_Programming_14_5_01-Tutorial but It seems to me that it needs ISE whereas I use Vivado 2013.4.

thanks very much.

best regards

Guillaume

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I am not familiar with the tutorials you are referring to. I think perhaps you are mixing the ZedBoard and the MicroZed board. Could you clarify which board you want to work with and post links to the tutorials you have used.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Gary.

    The board with which I work is MicroZed http://www.zedboard.org/product/microzed (without carrier board)

    I downloaded microzed tutorials at
    http://www.zedboard.org/documentation/1519.

    The first tutorial (tuto 1) is MicroZed_GettingStarted_v1.1.pdf (procedure to run a simple Linux design to show a Linux application running on the ARMu00AE dual-core Cortexu2122-A9 MPCoreu2122 Processing System (PS))

    The second tuto (tuto 2) I used is 01_MicroZed_Zynq_Intro_2013_2_01 at http://zedboard.org/content/vivado-20132-version-0

    Everything was all right but now I would like to implement a R/W register in PL, create a bitstream.bit, download the bitstream on ZYNQ and then used Linux as I did with tuto 1 to access to this register.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Gary.

    The board with which I work is MicroZed http://www.zedboard.org/product/microzed (without carrier board)

    I downloaded microzed tutorials at
    http://www.zedboard.org/documentation/1519.

    The first tutorial (tuto 1) is MicroZed_GettingStarted_v1.1.pdf (procedure to run a simple Linux design to show a Linux application running on the ARMu00AE dual-core Cortexu2122-A9 MPCoreu2122 Processing System (PS))

    The second tuto (tuto 2) I used is 01_MicroZed_Zynq_Intro_2013_2_01 at http://zedboard.org/content/vivado-20132-version-0

    Everything was all right but now I would like to implement a R/W register in PL, create a bitstream.bit, download the bitstream on ZYNQ and then used Linux as I did with tuto 1 to access to this register.