Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Increasing PYTHON 1300 frame rate by defining a ROI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 1013 views
  • Users 0 members are here
Related

Increasing PYTHON 1300 frame rate by defining a ROI

e14 Contributor
e14 Contributor over 9 years ago

I am developing an imaging solution using the ON PYTHON-1300-C Camera Module with the Microzed, and successfully tested the "embv_p1300c" reference design. I need to improve the frame rate by defining a region of interest (ROI). Only setting the camera register values for ROI did not improve the frame rate but trimmed the image showing the region outside the ROI as blank.

I would like to know what are the steps I need to follow to get this done using the "ON Semiconductor VITA Camera Receiver(3.2)" IP. Is there any documentation on usage of this IP?

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Yasuravithana,

    Try taking a look at these resources,

    http://community.avnet.com/t5/FMC-HDMI-I-O-VITA-Image-Sensor/reducing-the-frame-rate-of-a-VITA-2000-camera-to-30-FPS-using/m-p/16158/highlight/true#M537

    http://community.avnet.com/t5/FMC-HDMI-I-O-VITA-Image-Sensor/how-to-configure-the-higher-frame-rates/m-p/5556/highlight/true#M3

    http://community.avnet.com/t5/FMC-HDMI-I-O-VITA-Image-Sensor/FMC-IMAGEON-VITA-2000-at-1730-fps-rate/m-p/8119/highlight/true#M217

    https://www.xilinx.com/support/documentation/application_notes/xapp794-1080p60-camera.pdf

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Yasuravithana,

    Try taking a look at these resources,

    http://community.avnet.com/t5/FMC-HDMI-I-O-VITA-Image-Sensor/reducing-the-frame-rate-of-a-VITA-2000-camera-to-30-FPS-using/m-p/16158/highlight/true#M537

    http://community.avnet.com/t5/FMC-HDMI-I-O-VITA-Image-Sensor/how-to-configure-the-higher-frame-rates/m-p/5556/highlight/true#M3

    http://community.avnet.com/t5/FMC-HDMI-I-O-VITA-Image-Sensor/FMC-IMAGEON-VITA-2000-at-1730-fps-rate/m-p/8119/highlight/true#M217

    https://www.xilinx.com/support/documentation/application_notes/xapp794-1080p60-camera.pdf

    --Josh