Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed + FMC  control LEDs without Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 1494 views
  • Users 0 members are here
Related

MicroZed + FMC  control LEDs without Linux

nowksru
nowksru over 8 years ago

Hello,

My plan is to control LEDs on the FMC Carrier Card without installing any OS on the MicroZed (XC7Z020).

 

I first tried the FMC Carrier Card Linux User IO Tutorial , because it's apparently the only tutorial available for the MicroZed including the FMC-CC.

 

I did the tutorial step by step and also using the pre-built SD-Image. Both without any success. Only the "Power Good" (on the FMC-CC) and the power LED on the MicroZed switch on, but not the "DONE" LED on the FMC-CC. I also connected a terminal with teraterm, where nothing happened. For this tutorial I used Vivado 2013.3 as recommended.

 

 I am able to use the MicroZed by itself and control the LED on the MicroZed like in this tutorial. The steps I changed to try get it running on the FMC-CC are that I added the constraint file and I made 6 EMIO pins external inside Vivado for the FMC-CC and changed the pins that I controlled via xgpiops according to the MicroZed_HW_UG_v1_4.pdf in SDK. For this I used Vivado 2014.1 and did the programming using JTAG .

 

Am I missing a point? Is there any tutorial that someone can recommend me for achieving my goal?

 

Thanks in advance.

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Did you make a GPIO block in your Vivado block diagram? Also please share the constraints you used.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nowksru
    0 nowksru over 8 years ago in reply to jafoste4

    Hello,

    I only created the 'processing_system7_0' block, inside which I activated the 'EMIO GPIO (width)' with 6 IOs (4 LEDs + 2 buttons on the FMC-CC). In the block diagram I then made the 'GPIO_0' port of the PS external and renamed it to emio_user. These steps I made are the ones from the FMC Carrier Card Linux User IO Tutorial and I used the constraints provided within the tutorial.

     

    The constraints file only includes the necessary ports for the tutorial:

     

    # User IO
    #NET JX1_LED0     LOC = R19  | IOSTANDARD=LVCMOS18;  # "JX1_LED0"
    set_property PACKAGE_PIN R19 [get_ports {emio_user_tri_io[0]}]
    #NET JX1_LED1     LOC = V13  | IOSTANDARD=LVCMOS18;  # "JX1_LED1"
    set_property PACKAGE_PIN V13 [get_ports {emio_user_tri_io[1]}]
    #NET JX2_LED2     LOC = K16  | IOSTANDARD=LVCMOS18;  # "JX2_LED2"
    set_property PACKAGE_PIN K16 [get_ports {emio_user_tri_io[2]}]
    #NET JX2_LED3     LOC = M15  | IOSTANDARD=LVCMOS18;  # "JX2_LED3"
    set_property PACKAGE_PIN M15 [get_ports {emio_user_tri_io[3]}]
    #NET JX2_PB0      LOC = G19  | IOSTANDARD=LVCMOS18;  # "JX2_PB0"
    set_property PACKAGE_PIN G19 [get_ports {emio_user_tri_io[4]}]
    #NET JX2_PB1      LOC = G20  | IOSTANDARD=LVCMOS18;  # "JX2_PB1"
    set_property PACKAGE_PIN G20 [get_ports {emio_user_tri_io[5]}]

    set_property IOSTANDARD LVCMOS18 [get_ports {emio_user_tri_io[0]}]
    set_property IOSTANDARD LVCMOS18 [get_ports {emio_user_tri_io[1]}]
    set_property IOSTANDARD LVCMOS18 [get_ports {emio_user_tri_io[2]}]
    set_property IOSTANDARD LVCMOS18 [get_ports {emio_user_tri_io[3]}]
    set_property IOSTANDARD LVCMOS18 [get_ports {emio_user_tri_io[4]}]
    set_property IOSTANDARD LVCMOS18 [get_ports {emio_user_tri_io[5]}]

    # Bank 34, Vcco = 1.8V
    #set_property IOSTANDARD LVCMOS18 [get_ports -filter { IOBANK == 34 } ]

     

    -Urs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Urs, 

    I am assuming you set your VADJ on the carrier card to 1.8V?

    Have you taken a look at this?

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Using-the-MicroZed-Button-for-Input-Adam-Taylor-s-MicroZed/ba-p/393035

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nowksru
    0 nowksru over 8 years ago in reply to jafoste4

    Hi Josh,

    that is exactly the tutorial I was attempting. I actually just tried to do it again (MicroZed not connected to the FMC-CC) and noticed that the button is working (switch value changes from 0 to 1 on the console when pushed), but the LED never illuminates.

    I even tried to just switch it on with

    XGpioPs_WritePin(&Gpio, ledpin, toggle);

    inside the while loop, but didn't succeed.

     

    I set the VADJ jumper to 3V3 ( as its stated in the FMC Carrier Card Linux User IO Tutorial).

     

    -Urs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nowksru
    0 nowksru over 8 years ago in reply to nowksru

    XGpioPs_WritePin(&Gpio, ledpin, 1);

    is what I used to test the LED, not

    XGpioPs_WritePin(&Gpio, ledpin, toggle);

    This was a copy paste issue.

     

    -Urs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello URS,

    If your boards set to 3.3V you should change your constraitns to reflect this, from lvcmos18 to lvcmos33.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nowksru
    0 nowksru over 8 years ago in reply to jafoste4

    Hi Josh,

    I changed now all the from lvcmos18 entries inside the constraints file to lvcmos33, but it doesn't work either.

    I am also wondering, shouldn't the four LEDs on the FMC-CC at least switch off when I am running my configuration on the MicroZed? Because they are illuminating the whole time.

    Also I am still not able to illuminate the LED 'D3' on the Microzed. So far I am only able to read the state of the button on the MicroZed.

     

    To make sure, these are the pins I defined in the SDK for the EMIO pins:

    #define led_fmc 54
    #define led_fmc 55
    #define led_fmc 56
    #define led_fmc 57
    #define pbsw_fmc 58
    #define pbsw_fmc 59

     

    And these for the button and the LED 'D3' on the MicroZed:

    #define ledpin 47
    #define pbsw 51

     

    -Urs
     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nowksru
    0 nowksru over 8 years ago

    I managed now to control the LEDs on the FMC-CC via the PL, but still have no clue why it is not working via the PS.