Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed + FMC  control LEDs without Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 1497 views
  • Users 0 members are here
Related

MicroZed + FMC  control LEDs without Linux

nowksru
nowksru over 8 years ago

Hello,

My plan is to control LEDs on the FMC Carrier Card without installing any OS on the MicroZed (XC7Z020).

 

I first tried the FMC Carrier Card Linux User IO Tutorial , because it's apparently the only tutorial available for the MicroZed including the FMC-CC.

 

I did the tutorial step by step and also using the pre-built SD-Image. Both without any success. Only the "Power Good" (on the FMC-CC) and the power LED on the MicroZed switch on, but not the "DONE" LED on the FMC-CC. I also connected a terminal with teraterm, where nothing happened. For this tutorial I used Vivado 2013.3 as recommended.

 

 I am able to use the MicroZed by itself and control the LED on the MicroZed like in this tutorial. The steps I changed to try get it running on the FMC-CC are that I added the constraint file and I made 6 EMIO pins external inside Vivado for the FMC-CC and changed the pins that I controlled via xgpiops according to the MicroZed_HW_UG_v1_4.pdf in SDK. For this I used Vivado 2014.1 and did the programming using JTAG .

 

Am I missing a point? Is there any tutorial that someone can recommend me for achieving my goal?

 

Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Urs, 

    I am assuming you set your VADJ on the carrier card to 1.8V?

    Have you taken a look at this?

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Using-the-MicroZed-Button-for-Input-Adam-Taylor-s-MicroZed/ba-p/393035

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nowksru
    0 nowksru over 8 years ago in reply to jafoste4

    Hi Josh,

    that is exactly the tutorial I was attempting. I actually just tried to do it again (MicroZed not connected to the FMC-CC) and noticed that the button is working (switch value changes from 0 to 1 on the console when pushed), but the LED never illuminates.

    I even tried to just switch it on with

    XGpioPs_WritePin(&Gpio, ledpin, toggle);

    inside the while loop, but didn't succeed.

     

    I set the VADJ jumper to 3V3 ( as its stated in the FMC Carrier Card Linux User IO Tutorial).

     

    -Urs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nowksru
    0 nowksru over 8 years ago in reply to jafoste4

    Hi Josh,

    that is exactly the tutorial I was attempting. I actually just tried to do it again (MicroZed not connected to the FMC-CC) and noticed that the button is working (switch value changes from 0 to 1 on the console when pushed), but the LED never illuminates.

    I even tried to just switch it on with

    XGpioPs_WritePin(&Gpio, ledpin, toggle);

    inside the while loop, but didn't succeed.

     

    I set the VADJ jumper to 3V3 ( as its stated in the FMC Carrier Card Linux User IO Tutorial).

     

    -Urs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • nowksru
    0 nowksru over 8 years ago in reply to nowksru

    XGpioPs_WritePin(&Gpio, ledpin, 1);

    is what I used to test the LED, not

    XGpioPs_WritePin(&Gpio, ledpin, toggle);

    This was a copy paste issue.

     

    -Urs