Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed power via barrel jack
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 361 subscribers
  • Views 612 views
  • Users 0 members are here
Related

Microzed power via barrel jack

e14 Contributor
e14 Contributor over 12 years ago

Hello,

The hardware user guide for MicroZed mentions that the board can be powered using a 5V barrel jack connector while using as a stand-alone board (section 2.10.1). But I do not see how that is possible with the board at hand. Is there an additional/special port and connection cable that I need for this or does the 5V barrel jack input work only using a carrier card?

Thanks,

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    As discussed in section 2.10.1 of the Hardware Users Guide you would need to populate the Barrel Jack and associated capacitors in order to power the MicroZed in this manner:

     

    • Populate J4 barrel jack and use a 5V AC/DC supply rated for the projected current demand AND install the capacitors C212, C217, and C218.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks Gary,

    I wasn't sure what 'populate' meant until you highlighted it and so I confused that line as being related to J5 expansion header.

    Is there any place I can get additional info about what specific components I should populate those connections with? I do see I need a 4 pinned barrel jack connector there but I can't find one? Also where can I find the capacitors I need (what F etc).

    Thanks,
    Onur


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks Gary,

    I wasn't sure what 'populate' meant until you highlighted it and so I confused that line as being related to J5 expansion header.

    Is there any place I can get additional info about what specific components I should populate those connections with? I do see I need a 4 pinned barrel jack connector there but I can't find one? Also where can I find the capacitors I need (what F etc).

    Thanks,
    Onur