Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed power via barrel jack
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 361 subscribers
  • Views 611 views
  • Users 0 members are here
Related

Microzed power via barrel jack

e14 Contributor
e14 Contributor over 12 years ago

Hello,

The hardware user guide for MicroZed mentions that the board can be powered using a 5V barrel jack connector while using as a stand-alone board (section 2.10.1). But I do not see how that is possible with the board at hand. Is there an additional/special port and connection cable that I need for this or does the 5V barrel jack input work only using a carrier card?

Thanks,

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The MicroZed Bill of Materials (BOM) is available for download at this link: http://zedboard.org/support/documentation/1519

     

    Select the board version you have and look for J4 and C212, C217 and C218. They will be listed as DNP (Do Not Populate) on the BOM but the  values and part numbers will be specified.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The MicroZed Bill of Materials (BOM) is available for download at this link: http://zedboard.org/support/documentation/1519

     

    Select the board version you have and look for J4 and C212, C217 and C218. They will be listed as DNP (Do Not Populate) on the BOM but the  values and part numbers will be specified.

     

    -Gary