Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed daughterboard with 2nd PHY?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 362 subscribers
  • Views 781 views
  • Users 0 members are here
Related

MicroZed daughterboard with 2nd PHY?

100kenc
100kenc over 9 years ago

Hi,

I would like to use the second eth MAC in the Zync. Are there any MicroZed daughterboards available for this?

I was planning to modify this http://www.freertos.org/FreeRTOS-Plus/FreeRTOS_Plus_TCP/TCPIP_FAT_Examples_Xilinx_Zynq.html

for 2 ethernet ports, but I could not find Zync boards with 2 ETH PHYs. I already have 1 MicroZed board, so a daughterboard with an additional PHY connected to the second ETH MAC would be nice.

Thanks,

Ken 

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Ken,

    Try taking a look at the Ethernet FMC over at this link

    http://ethernetfmc.com/exampledesigns/

    There is also an example design already done on the MicroZed to help you get started.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100kenc
    0 100kenc over 9 years ago in reply to jafoste4

    Hi Josh, I have one more question about this.

    According to the MIO table from Xilinx, I can use MIO pins 28 to 39 to connect to ETH1 if I don't need USB0. In that case I don't need to route ETH1 to EMIO pins via the PL.

    Is that correct?

    regards,

    Ken

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100kenc
    0 100kenc over 9 years ago in reply to jafoste4

    Hi Josh, I have one more question about this.

    According to the MIO table from Xilinx, I can use MIO pins 28 to 39 to connect to ETH1 if I don't need USB0. In that case I don't need to route ETH1 to EMIO pins via the PL.

    Is that correct?

    regards,

    Ken