Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed Carrier Design Guide
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 803 views
  • Users 0 members are here
Related

MicroZed Carrier Design Guide

e14 Contributor
e14 Contributor over 12 years ago

We have just posted the MicroZed Carrier Design Guide to assist the community in designing and developing custom carrier cards for MicroZed.  This is a living and breathing document, so please reply to this post with any suggestions or desired additions.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    An updated version of this documents has been posted here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ghalady
    0 ghalady over 12 years ago

    Tried accessing the Design Guide was not able to open the document. Question I had was is it possible to debug the PL designs on Microzed Zync7010 using USB cable and Chipscope

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to ghalady

    The link at the top of the post was replaced by the newer version. You can just go to the MicroZed Documentation page and download the newest version: http://www.zedboard.org/documentation/1519

     

    Sorry for the problem.

     

    Yes, you can debug PL designs on MicroZed. You will need a JTAG Programming Cable (Xilinx Platform Cable,Digilent HS1 or HS2 Cable. If you don't already have a JTAG Cable we recommend the Digilent HS2 Cable: http://www.em.avnet.com/en-us/design/drc/Pages/Digilent-JTAG-HS2-Programming-Cable.aspx

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    What is the tolerance on the 5V input from the carrier? Can anyone verify that powering with 5.5V would be OK? 

    On a cursory inspection it seems to primarily go to a switcher, which can accept a reasonable range. What am I missing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 12 years ago

    The tolerance requirement is 10%, based on the max Vin of the MAX6037A voltage reference.  The max Vin of that device is 5.5V, so while you u201Ccouldu201D run it at 5.5V, you are pushing the limits.  The absolute max on the pins of the 6037 is 6V, but the max operating range is stated at 5.5V.

    One thing to consider would be that if you are NOT using the XADC header, you could remove L1 from the board.  Doing so would disconnect the input to the MAX6037 and the MAX8891, which only generate the reference voltage and 1.8V used by the XADC header.
    Thanks
    Chris