Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed Carrier Design Guide
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 804 views
  • Users 0 members are here
Related

MicroZed Carrier Design Guide

e14 Contributor
e14 Contributor over 12 years ago

We have just posted the MicroZed Carrier Design Guide to assist the community in designing and developing custom carrier cards for MicroZed.  This is a living and breathing document, so please reply to this post with any suggestions or desired additions.

  • Sign in to reply
  • Cancel
Parents
  • ctammann
    0 ctammann over 12 years ago

    The tolerance requirement is 10%, based on the max Vin of the MAX6037A voltage reference.  The max Vin of that device is 5.5V, so while you u201Ccouldu201D run it at 5.5V, you are pushing the limits.  The absolute max on the pins of the 6037 is 6V, but the max operating range is stated at 5.5V.

    One thing to consider would be that if you are NOT using the XADC header, you could remove L1 from the board.  Doing so would disconnect the input to the MAX6037 and the MAX8891, which only generate the reference voltage and 1.8V used by the XADC header.
    Thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ctammann
    0 ctammann over 12 years ago

    The tolerance requirement is 10%, based on the max Vin of the MAX6037A voltage reference.  The max Vin of that device is 5.5V, so while you u201Ccouldu201D run it at 5.5V, you are pushing the limits.  The absolute max on the pins of the 6037 is 6V, but the max operating range is stated at 5.5V.

    One thing to consider would be that if you are NOT using the XADC header, you could remove L1 from the board.  Doing so would disconnect the input to the MAX6037 and the MAX8891, which only generate the reference voltage and 1.8V used by the XADC header.
    Thanks
    Chris