Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Building MicroZed hardware in Vivado problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 362 subscribers
  • Views 1113 views
  • Users 0 members are here
Related

Building MicroZed hardware in Vivado problem

e14 Contributor
e14 Contributor over 12 years ago

When using Vivado 2013.4 to build the MicroZed hardware(following tutorial 1 located at http://www.zedboard.org/design/1519/10), I get the following:

WARNING: [IP_Flow 19-2987] IP 'System_processing_system7_0_0' with unlicensed IP definition 'xilinx.com:ip:processing_system7:5:3' depends on licensed subcore IP definition 'xilinx.com:ip:processing_system7_bfm:2.0' Please update your IP definition with license information.

WARNING: [xilinx.com:ip:processing_system7:5.3-1] System_processing_system7_0_0: The Zync BFM requires an AXI BFM license to run. Please ensure that you have purchased and setup the AXI BFM license prior to running simulation with this block. Please contact your Xilinx sales office for more information on puchasing this license.

I'm not sure what I should be doing about this.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You selected the Zynq7 Processing System BFM (Bus Functional Model) when you added your initial IP to the block design rather than the Zynq7 Processing System IP.

     

    The Bus Functional Model does require an additional license.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You selected the Zynq7 Processing System BFM (Bus Functional Model) when you added your initial IP to the block design rather than the Zynq7 Processing System IP.

     

    The Bus Functional Model does require an additional license.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I rebuilt to make sure- selecting the ZYNQ7 Processing System (second choice from the bottom of the list) results in the aforementioned warnings. Was there a change between 2013.2 and 2013.4 that would cause that? There is a small difference between the tutorial and what I see; in the tutorial, the block diagram on page 10 is labled "processing_system7_1", whereas the one on my computer is labled "processing_system7_0". I don't know if this makes a difference or if there are other changes as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    There are some differences between 2013.2 and 2013.4, such as the fact that the MicroZed board is included as a preset in 2013.4 and you do not need to load the board awareness files. You should use the built in MicroZed presets for 2013.4. The different appended _0 or _1 to the IP should have no real impact except that you might need to adjust the parameter names to match in any software written with one of the versions in mind.

     

    I am not sure why you are having an issue if you are really selecting Zynq7 Processing System, I just tried it and it works fine in Vivado 2013.4. I would suggest starting over with a new project.

     

    -Gary