Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design JX1/JX2 Track Impedance
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 361 subscribers
  • Views 1043 views
  • Users 0 members are here
Related

JX1/JX2 Track Impedance

e14 Contributor
e14 Contributor over 12 years ago

One of the selling points of the MicroZed is the high quality high frequency connectors JX2 and JX2, since unlike many boards they allow many high frequency signals to be connected to the Zynq.


I'd like to ensure high speed signal integrity for signals going from a carrier board through JX 1 and JX2 to the Zynq. The key parts are the Zynq input pin standard (LVDS etc) and the track impedance on the carrier board (my responsibility) and the track impedance for the 2" tracks on the MicroZed board. At GHz bit rates, a 2" track is electrically long, and simulations show the difference between 40ohms and 80ohms is significant.


Now the DDR tracks are 40ohms, but what's the "typical" impedance of the tracks from the JX1/2 connectors? N.B. I'm neither after specifications nor guarantees, but I would like an indication of likely impedance.


If that isn't known, what's the track width and pre-preg thickness, and I'll make a guesstimate from that.


Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Sorry for the confusion. The documentation he is referring to is in the Carrier Card Users Guides, both the MicroZed IO Carrier Card and the MicroZed FMC Carrier Card, in the 'Layout Routing Guidelines' sections.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Sorry for the confusion. The documentation he is referring to is in the Carrier Card Users Guides, both the MicroZed IO Carrier Card and the MicroZed FMC Carrier Card, in the 'Layout Routing Guidelines' sections.

     

    -Gary