Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Ethernet - MIO - 3.3V supply
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 360 subscribers
  • Views 1219 views
  • Users 0 members are here
Related

Ethernet - MIO - 3.3V supply

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I'm a bit confused about the supplying voltage of the zynq MIO with ethernet. I bought a carrier breakout board with my microzed and I can set the supply of VCCIO to either 3.3V, 2.5V or 1.8V. For compatibility, I must use 3.3V, but inside the Zynq TRM at section "16.6.7 MIO Pin Considerations", I can read "LVCMOS33 is not supported for the RGMII interface. Recommendation is to use 1.8/2.5V I/O
standards." The VCCIO supplied the MIO bank and the ethernet is connected to it. So, it's been a while I used the microzed before I read this... But I've got no problem yet using 3.3V, is it normal ? Should I use the 2.5V for safety ?

Thanks !

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    The VCCIO that you can control is for the PL I/O banks, not the MIO.The Vcco_mio is fixed and regulated on the MicroZed. On MicroZed, the Ethernet is tied to MIO Bank 1, which is fixed at 1.8V. See the MicroZed UG for more information.

     

    Bryan