Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Boot loop with USB power supply on DC barrel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 1359 views
  • Users 0 members are here
Related

Boot loop with USB power supply on DC barrel

e14 Contributor
e14 Contributor over 8 years ago

I've encountered an power supply issue with microZed Soc. I'm trying to power the board using USB charger/Battery back. It worked fine through the UART USB port. But if I connect it through the DC barrel jack or VIN_HDR on the expansion header, the boot process will end up in a reset loop. Caps 212 217 218 are depopulated.

The reset happens after PL configuration and before entry to the OS. The multimeter show a significant voltage drop at the precise moment.

I've checked the schematics of the board design (rev F). Power through UART and VIN_HDR is no different. I've also included a polyzen on my carrier card.

Can someone shed some light on this?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    OK, I did some testing with oscilloscope.

    image

    VIN_HDR during power on using a powerful adapter


    image

    With any USB charger (this one 3A rating) shows a voltage drop every 0.45s. Thus giving a boot loop


    image

    The same USB charger inserted to UART port shows a smooth power up. In fact, a 500mA regular USB port will also work.

    I have two microzed and both of them experience the same problem. So I think it's a design issue. Can someone shed some light on this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    OK, I did some testing with oscilloscope.

    image

    VIN_HDR during power on using a powerful adapter


    image

    With any USB charger (this one 3A rating) shows a voltage drop every 0.45s. Thus giving a boot loop


    image

    The same USB charger inserted to UART port shows a smooth power up. In fact, a 500mA regular USB port will also work.

    I have two microzed and both of them experience the same problem. So I think it's a design issue. Can someone shed some light on this?