Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Boot loop with USB power supply on DC barrel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 1357 views
  • Users 0 members are here
Related

Boot loop with USB power supply on DC barrel

e14 Contributor
e14 Contributor over 8 years ago

I've encountered an power supply issue with microZed Soc. I'm trying to power the board using USB charger/Battery back. It worked fine through the UART USB port. But if I connect it through the DC barrel jack or VIN_HDR on the expansion header, the boot process will end up in a reset loop. Caps 212 217 218 are depopulated.

The reset happens after PL configuration and before entry to the OS. The multimeter show a significant voltage drop at the precise moment.

I've checked the schematics of the board design (rev F). Power through UART and VIN_HDR is no different. I've also included a polyzen on my carrier card.

Can someone shed some light on this?

 

Thanks!

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    When you power your  board via a wall jack does it operate correctly in both scenarios?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to jafoste4

    If through an DC adapter that is fine. But I don't have access to that in the field. Only 5V battery pack or USB charger on a car.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    I'm suspecting some stray capacitance associated with Vin_HDR net. It's very reproducible.

    Any idea how to solve it? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    OK, I did some testing with oscilloscope.

    image

    VIN_HDR during power on using a powerful adapter


    image

    With any USB charger (this one 3A rating) shows a voltage drop every 0.45s. Thus giving a boot loop


    image

    The same USB charger inserted to UART port shows a smooth power up. In fact, a 500mA regular USB port will also work.

    I have two microzed and both of them experience the same problem. So I think it's a design issue. Can someone shed some light on this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    Forum editor could not display my inserted image

    three images in order described in the last comment

    https://www.dropbox.com/s/o35ibola1dv10uq/T0000.PNG

    https://www.dropbox.com/preview/Public/uZed_issues/TEK00006.PNG

    https://www.dropbox.com/preview/Public/uZed_issues/TEK00009.PNG

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    still no one?  I've try power it using both side and then unplug the UART. It still resets.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    Can any FAE from zedboard help me on this issue? It's been months without reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 8 years ago

    Hi, sorry for the late response here. Are you connected to the USB UART at the same time as power is being provided through Vin header? Is anything else being powered by Vin header on your carrier board? Adding back the bulk capacitance to the board may help with the voltage drop, which may be why the board is resetting. You could also try shorting D9. The UART should still be protected and you shouldn't have to worry about backfeed into the 5V from the barrel jack or carrier as long as the output voltage stays at 5V.

    The first thing I would try is adding bulk capactiance to the Vin header node. Also verify that power is only coming from the Vin header and not from the UART port. The diodes D9 and D4 are there to protect the potential power sources, if you can assure you are only using one or the other then you can short these. Another option would be to short D9 and open D4 which would guarantee power from the DC source. Please give these a try and let me know if the problem persists.

    Thanks

    Chris