Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Boot loop with USB power supply on DC barrel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 1357 views
  • Users 0 members are here
Related

Boot loop with USB power supply on DC barrel

e14 Contributor
e14 Contributor over 8 years ago

I've encountered an power supply issue with microZed Soc. I'm trying to power the board using USB charger/Battery back. It worked fine through the UART USB port. But if I connect it through the DC barrel jack or VIN_HDR on the expansion header, the boot process will end up in a reset loop. Caps 212 217 218 are depopulated.

The reset happens after PL configuration and before entry to the OS. The multimeter show a significant voltage drop at the precise moment.

I've checked the schematics of the board design (rev F). Power through UART and VIN_HDR is no different. I've also included a polyzen on my carrier card.

Can someone shed some light on this?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • ctammann
    0 ctammann over 8 years ago

    Hi, sorry for the late response here. Are you connected to the USB UART at the same time as power is being provided through Vin header? Is anything else being powered by Vin header on your carrier board? Adding back the bulk capacitance to the board may help with the voltage drop, which may be why the board is resetting. You could also try shorting D9. The UART should still be protected and you shouldn't have to worry about backfeed into the 5V from the barrel jack or carrier as long as the output voltage stays at 5V.

    The first thing I would try is adding bulk capactiance to the Vin header node. Also verify that power is only coming from the Vin header and not from the UART port. The diodes D9 and D4 are there to protect the potential power sources, if you can assure you are only using one or the other then you can short these. Another option would be to short D9 and open D4 which would guarantee power from the DC source. Please give these a try and let me know if the problem persists.

    Thanks

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ctammann
    0 ctammann over 8 years ago

    Hi, sorry for the late response here. Are you connected to the USB UART at the same time as power is being provided through Vin header? Is anything else being powered by Vin header on your carrier board? Adding back the bulk capacitance to the board may help with the voltage drop, which may be why the board is resetting. You could also try shorting D9. The UART should still be protected and you shouldn't have to worry about backfeed into the 5V from the barrel jack or carrier as long as the output voltage stays at 5V.

    The first thing I would try is adding bulk capactiance to the Vin header node. Also verify that power is only coming from the Vin header and not from the UART port. The diodes D9 and D4 are there to protect the potential power sources, if you can assure you are only using one or the other then you can short these. Another option would be to short D9 and open D4 which would guarantee power from the DC source. Please give these a try and let me know if the problem persists.

    Thanks

    Chris