Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed Preset TCL Files
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 362 subscribers
  • Views 1053 views
  • Users 0 members are here
Related

Microzed Preset TCL Files

e14 Contributor
e14 Contributor over 8 years ago

I am attempting to create a board design using Vivado 2016.2 with a Microzed 7020 and FMC Carrier Card.

 

I cannot find a Preset for the ZYNQ7 Processing System. 

 

I am using the Board Definition Files located at

http://zedboard.org/content/board-definition-files-0

but that contains a file, preset.xml which is not a valid preset since Vivado expects a TCL file.

 

I also tried downloading the preset : MicroZed Zynq PS Preset for Vivado 2013.4 (TCL)

but Vivado says that is not a valid preset either.

 

Is there a Zynq PS preset for Vivado 2016.2?

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    Did you install the BDF labeled MicroZed Board Definition Install for Vivado 2015.3 through 2017.4

    and what directory did you install it in?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to jafoste4

    Hi,
    I have the same problem. I installed the BDF labeled files for Vivado 2015 to 2017.4, but I am not able to see the microzed in the preset menu while configuring the PS. Still, I am able to see the zedboard ones.

    I triede to source the tcl script MicroZed_PS_properties_v03.tcl , but then I got an error during bitstream generation.

    What can I do to solve this?

    Andrea

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to jafoste4

    Hi,
    I have the same problem. I installed the BDF labeled files for Vivado 2015 to 2017.4, but I am not able to see the microzed in the preset menu while configuring the PS. Still, I am able to see the zedboard ones.

    I triede to source the tcl script MicroZed_PS_properties_v03.tcl , but then I got an error during bitstream generation.

    What can I do to solve this?

    Andrea