Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design No Output to Console
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 459 views
  • Users 0 members are here
Related

No Output to Console

e14 Contributor
e14 Contributor over 12 years ago

Hello,

In Xilinx ISE 14.5, I made a simple design (using the MicroZed board), where I just instantiated the Processor System and connected the DDR, MIO and PS signals to the FPGA pins.
I defined the .ucf according to the schematic on MicroZed_RevF_Schematic_140128.pdf.
On Xilinx Platform Studio, I enabled the peripherals: UART1, GPIO0, SD0, USB0, Enet0 and QuadSPI Flash Memory Interface, according to table 19 on MicroZed_HW_UG_V1_2.pdf and exported the HW design to SDK.
I installed the u201CCP210x USB to UART Bridge VCP Driveru201D and on Xilinx SDK I followed the steps described on 02_MicroZed_Zynq_Hello_World_2013_2_01.pdf
starting from generating the Board Support Package (the ps_hw_platform was already generated).
Everything seems to be ok (the configuration runs without errors, the LED D3 is switched off) except the output to terminal. I cannot see anything on SDK console. I also tried with TeraTerm the same configurations and I do not see nothing on it.

What could be missing on my design/setup?

Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The first thing to try is to push the RST button on the MicroZed board or restart the application from SDK after you have loaded your design as described but not seen the terminal output you expected. It could be that the terminal output was completed by the time you opened up your TeraTerm session. Also make sure TeraTerm is set to the correct com port and baud rate.

     

    Otherwise, you might try the MicroZed tutorial solutions files to make sure your setup is good with a known good design. You can find the solution archives here: http://www.zedboard.org/design/1519/10

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    It is working.
    It seems that I had something misconfigured.

    Thank you