Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design No Output to Console
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 461 views
  • Users 0 members are here
Related

No Output to Console

e14 Contributor
e14 Contributor over 12 years ago

Hello,

In Xilinx ISE 14.5, I made a simple design (using the MicroZed board), where I just instantiated the Processor System and connected the DDR, MIO and PS signals to the FPGA pins.
I defined the .ucf according to the schematic on MicroZed_RevF_Schematic_140128.pdf.
On Xilinx Platform Studio, I enabled the peripherals: UART1, GPIO0, SD0, USB0, Enet0 and QuadSPI Flash Memory Interface, according to table 19 on MicroZed_HW_UG_V1_2.pdf and exported the HW design to SDK.
I installed the u201CCP210x USB to UART Bridge VCP Driveru201D and on Xilinx SDK I followed the steps described on 02_MicroZed_Zynq_Hello_World_2013_2_01.pdf
starting from generating the Board Support Package (the ps_hw_platform was already generated).
Everything seems to be ok (the configuration runs without errors, the LED D3 is switched off) except the output to terminal. I cannot see anything on SDK console. I also tried with TeraTerm the same configurations and I do not see nothing on it.

What could be missing on my design/setup?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    It is working.
    It seems that I had something misconfigured.

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    It is working.
    It seems that I had something misconfigured.

    Thank you