Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design New USB-UART connection
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 361 subscribers
  • Views 1532 views
  • Users 0 members are here
Related

New USB-UART connection

e14 Contributor
e14 Contributor over 9 years ago
I have been working with a microZed board that is connected via jtag to my pc. I have configured the microZed board settings in Vivado 2014.4 for this, but now I want to use a new usb uart connection from my pc to the microZed board in addition to the jtag connection. I have enabled the uart port in Vivado, and installed the driver "Silicon Labs CP210x USB-to-UART" online, but still neither the microZed board or the port is appearing on device manager. Any suggestions?
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    The MicroZed board in the evaluation kit is a 'standard' MicroZed and does have the USB-UART functionality.

    The SiLabs driver normally installs automatically in Windows 7, as mentioned above, it can take a really long time the first time. You might want to uninstall the driver you installed and let the USB-UART driver install automatically if you can.

    The other thing to check would be the USB port you have connected your MicroZed to. Make sure it can supply enough power for the MicroZed to operate (so no 'passive' or un-powered USB hubs). If you could try a different USB port, or even better a different Host PC, that could rule out any issues with your MicroZed board or cable.

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    I have tried to let my PC automatically install the needed driver but nothing pops up on device manager. I have tried with multiple PCs and USB ports. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    I have tried to let my PC automatically install the needed driver but nothing pops up on device manager. I have tried with multiple PCs and USB ports.