Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design New USB-UART connection
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 361 subscribers
  • Views 1736 views
  • Users 0 members are here
Related

New USB-UART connection

e14 Contributor
e14 Contributor over 10 years ago
I have been working with a microZed board that is connected via jtag to my pc. I have configured the microZed board settings in Vivado 2014.4 for this, but now I want to use a new usb uart connection from my pc to the microZed board in addition to the jtag connection. I have enabled the uart port in Vivado, and installed the driver "Silicon Labs CP210x USB-to-UART" online, but still neither the microZed board or the port is appearing on device manager. Any suggestions?
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The blue LED, D2, only turns on once the Zynq PL (Programmable Logic) section has been configured. This would only occur under software program control while booting from QSPI or SD Card memory, or manually via JTAG. If you have set the boot mode jumpers, JT1 - JT2 - JT3 to the JTAG position (all 3 in the 1-2 position) this should not occur unless you are loading the PL from the JTAG interface. You could make sure that you have set the boot jumpers correctly or even just remove the JTAG adapter from the MicroZed J3 connector . If the blue LED still turns on then either there is a problem with the boot jumpers or the circuit that drives D2.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The blue LED, D2, only turns on once the Zynq PL (Programmable Logic) section has been configured. This would only occur under software program control while booting from QSPI or SD Card memory, or manually via JTAG. If you have set the boot mode jumpers, JT1 - JT2 - JT3 to the JTAG position (all 3 in the 1-2 position) this should not occur unless you are loading the PL from the JTAG interface. You could make sure that you have set the boot jumpers correctly or even just remove the JTAG adapter from the MicroZed J3 connector . If the blue LED still turns on then either there is a problem with the boot jumpers or the circuit that drives D2.

     

    -Gary