Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design red led never turns off
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 362 subscribers
  • Views 714 views
  • Users 0 members are here
Related

red led never turns off

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I have a microzed with xc7z020, the red led never turns off, is that normal?

Also, I can only program the FPGA when the jumpers are all configured up.

When using another board, after powering the red led is off, so I don't know what is wrong with the first board.

Any ideas?

Thanks.

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hi iahmed,

    The red led only goes off after the MIO pins have been configured during first stage of the boot process. 

    If you are trying to boot from QSPI Flash, perhaps your QSPI data has been corrupted somehow on that MicroZed where you do no see the LED go off.

    There is a 7020 version of the "Open Source Linux In System QSPI Programming Tutorial" that you can use to try and boot your MicroZed from the microSD card.

    http://microzed.org/support/design/1519/10

    If you can get that image to boot with SD card boot mode jumper settings, that design will also restore your QSPI Flash back to the factory image.

    If you have questions about what jumper settings to use, please refer back to the MicroZed Hardware User Guide:

    http://microzed.org/support/documentation/1519

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    Thanks Kevin for your feedback.
    Yes this board has First Stage Boot Loader (FSBL) created as in the following link:
      http://forums.xilinx.com/t5/Xcell-Daily-Blog/A-Boot-Loader-for-MicroZed-Adam-Taylor-s-MicroZed-Chronicles/ba-p/378855

    Is the way you described will remove such boot loader and restore the QSPI flash back to the factory image?

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hi iahmed,

    Yes, if you are following Adam's instructions from the beginning then there should be no problems as long as you are not skipping steps.  Adam uses the "MicroZed_PS_properties_v02.tcl" file from the MicroZed.org Documentation page (there is a newer version available today but they both should work okay) in this earlier post here:

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Bringing-up-the-Avnet-MicroZed-with-Vivado/ba-p/362901

    Yes, the image that I pointed out earlier will reset your board back to the factory QSPI Flash image.

    Regards,

    -Kevin