Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design red led never turns off
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 362 subscribers
  • Views 713 views
  • Users 0 members are here
Related

red led never turns off

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I have a microzed with xc7z020, the red led never turns off, is that normal?

Also, I can only program the FPGA when the jumpers are all configured up.

When using another board, after powering the red led is off, so I don't know what is wrong with the first board.

Any ideas?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi iahmed,

    Yes, if you are following Adam's instructions from the beginning then there should be no problems as long as you are not skipping steps.  Adam uses the "MicroZed_PS_properties_v02.tcl" file from the MicroZed.org Documentation page (there is a newer version available today but they both should work okay) in this earlier post here:

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Bringing-up-the-Avnet-MicroZed-with-Vivado/ba-p/362901

    Yes, the image that I pointed out earlier will reset your board back to the factory QSPI Flash image.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi iahmed,

    Yes, if you are following Adam's instructions from the beginning then there should be no problems as long as you are not skipping steps.  Adam uses the "MicroZed_PS_properties_v02.tcl" file from the MicroZed.org Documentation page (there is a newer version available today but they both should work okay) in this earlier post here:

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Bringing-up-the-Avnet-MicroZed-with-Vivado/ba-p/362901

    Yes, the image that I pointed out earlier will reset your board back to the factory QSPI Flash image.

    Regards,

    -Kevin