Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed vision carrier card camera extender
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 943 views
  • Users 0 members are here
Related

Microzed vision carrier card camera extender

kcox@sgss.com
kcox@sgss.com over 8 years ago

Hi

 

I have purchased a PCIE camera extender cable from SAMTEC for the Microzed Embedded Vision Carrier card.  I'm trying to extend the Python 1300C camera module.  The SAMTEC part number is PCIEC-064-0100-EC-EM-P-85.  064 = x4 lane width,  0100 = 100 mm length,  EC-EM=two connectors, P=Eye speed cable and power lines, 85=85 Ohm impedance.  When I try to use the extender cable I can here a click from the card and the power light to the carrier card goes out.  No other lights come on from the attached Microzed card or the carrier card.  The click sounds like a relay and is very faint.  The hardware design guide for the carrier card says an extender card should work.  The only options for the cable that I was not sure about were the cable option.  My choices were:

  P  (which I picked), eye speed with power

  C   eye speed Copper

  CP eye speed copper with power.

I have two cables and they both exhibit same symptoms.  Has anyone successfully exentended the Python Camera module on this carrier card?

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Dan,

    The Samtec cable and the Python 1300 camera module are not compatible. The pinout on the Python 1300 camera module does not follow the standard PCIe pinout. If you still wish to use the module, most likely a custom cable would need to be developed. Are you currently talking to your local Avnet FAE?

     

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Dan,

    The Samtec cable and the Python 1300 camera module are not compatible. The pinout on the Python 1300 camera module does not follow the standard PCIe pinout. If you still wish to use the module, most likely a custom cable would need to be developed. Are you currently talking to your local Avnet FAE?

     

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rockytop
    0 rockytop over 8 years ago in reply to jafoste4

    I exchanged e-mail with someone this morning at Avnet, but not sure he is the local FAE. What's the best way to find out who this is and contact them? 

    What's your experience with extension cables - shielded or unsheilded? Flat or round?