Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design microzed carrier board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 361 subscribers
  • Views 685 views
  • Users 0 members are here
Related

microzed carrier board

e14 Contributor
e14 Contributor over 11 years ago

can the pmod header or other I/O pin on carrier board accept ttl 5v? or only upto 3.3

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Only 3.3V. In most cases these I/O pins are connected directly to the Zynq device. Based on the Zynq data sheet the max voltage on any PL I/O pin is: VCCO + 0.20V.

     

    http://www.xilinx.com/support/documentation/data_sheets/ds187-XC7Z010-XC7Z020-Data-Sheet.pdf

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I made a custom carrier board and the QSPI does not seem to be working properly. This is interesting because nothing on my carrier touches the QSPI...

    When probing some of the Reset lines, I notice that on the Avnet Carrier board, the SRST line drops to zero briefly (~1ms) after it finishes ramping on bootup.
    For my carrier board, the SRST is not dropping down to zero briefly. I feel like this has something to do with the QSPI not working as it is the RST# line of the QSPI Chip U7 pin9

    Any tips would be fantastic, thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I am sorry, I said QSPI Chip U7 pin9 but I means Qspi Chip U7 pin A4.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    How have you connected the PG_MODULE signal? Are all your power supplies coming up as expected?
    Bryan