Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design PL to PS Interrupt
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 362 subscribers
  • Views 2874 views
  • Users 0 members are here
Related

PL to PS Interrupt

raymadigan
raymadigan over 10 years ago

I am trying to implement simple PL to PS interrupt using the IRQ_F2P line on the Zynq.   I have an AXI Lite component that exports a pin with single pin interface as interrupt.  I can watch it go high in an ILA for a single clock cycle when I want the interrupt to run.

 

On the PS I have the following code:

#define INTC_DEVICE_ID XPAR_SCUGIC_0_DEVICE_ID
 
  ////#define XPS_FPGA0_INT_ID 61U from xparameters.h
#define INTC_DEVICE_INT_ID XPS_FPGA0_INT_ID
 
  Status = XScuGic_Connect(&InterruptController, INTC_DEVICE_INT_ID,
                                                   (Xil_ExceptionHandler)DeviceDriverHandler,
                                                   (void *)&InterruptController);
   
  // If I simulate the interrupt without pulling the interrupt pin high it seems to work
 
   Status = XScuGic_SoftwareIntr(&InterruptController,
 
                                                           INTC_DEVICE_INT_ID,
 
                                                           XSCUGIC_SPI_CPU0_MASK);
 
    
 
   But it doesn't work with the real interrupt.  This is supposed to be easy, is there something I didn't do?  
 
   I can show all of the code, it is basically the example from he ScuGic example in the SDK.
 
    
 
   Thanks
  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Raymadigan,

    If you haven't yet I would suggest going through our ZynqHW lab Speedways. In those speedway labs we implement a PL to PS interrupt using the IRQ_F2P. At the very least I would compare that setup to your own.

    http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-hardware-vivado-20133-and-201441

    Also what Vivado/SDK version are you using?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • raymadigan
    0 raymadigan over 10 years ago in reply to jafoste4

    I thought I did but will do it again, I wasn't sure how it is restructured.  The link you send doesn't work.  I will see what I can, if you could point me to the right place I would appreciate it.

     

    I am using windows 10 and vivado 2016.2

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago

    Hi Raymadigan,

    Sorry about that, here is the link

     http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-hardware-vivado-20133-and-201441

    Also note that you will need the correct vivado version to complete this lab. On another note we are going to be posting a 2016.2 revision of these labs shortly. Your error kind of reminds me of an issue I had when I was in the process of updating these labs. I'll refer you to a post that I responded to that may be of assistance. Please see bottom two posts.

    http://zedboard.com/content/speedway-lab-10-difficulties

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • raymadigan
    0 raymadigan over 10 years ago

    Josh,

    Thanks for your response.  I found the Auto Infer Interface yesterday so I went back to make sure I didn't mess that up.  This pin is listed in the Ports and Interface section as an expandable element.  In the interface mode it has master and nothing else is marked.  When I expand it the pin has direction out and type name is std_logic.

    In the IP I have two of these pins, nothing is connected to the second but it is exactly the same.  I had this connected to a concat but it didn't work and to try to see why I disconnected it.  I am in the process of totally removing it to make it easier to see what is going wrong.

    To do the PS side I copied the code from the xilinx sdk examples and what they had is nearly the same as the speedway workshop.   The only difference is a call to Xil_ExceptionInit(); before XIL_ExceptionRegisterHandler(...);  

     

    One difference is that the IP that I am using to generate the interrupt is an AXI Lite IP That I use to transfer small data chunks between the PS and the PL.  I want to use the interrupts to signal when data is ready so the PS doesn't have to poll.

     

    My next step is to build a small version that only does what I need that is isolated from the rest of my application to help isolate the issue.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • raymadigan
    0 raymadigan over 10 years ago

    I built a board with only the AXI Lite component that when a 1 is sent to register 0 it pulls an exported line high for one clock cycle.  The line is auto inferred to be an interrupt.  I can watch the line go high in an ILA.  Still the interrupt doesn't file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • raymadigan
    0 raymadigan over 10 years ago in reply to raymadigan

    I found the problem, Something I missed when I read the Speedway work twice, :(.  I wasn't setting the priority correct.  When I just used your values it worked in the isolated case and I suspect it will work in the product.  Thanks for all of your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago in reply to raymadigan

    Hi Raymadigan,

    Glad to hear! I appreciate you posting your solution as well. Hopefully it will help someone else in the future.

    --Josh