Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design PL to PS Interrupt
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 362 subscribers
  • Views 2874 views
  • Users 0 members are here
Related

PL to PS Interrupt

raymadigan
raymadigan over 10 years ago

I am trying to implement simple PL to PS interrupt using the IRQ_F2P line on the Zynq.   I have an AXI Lite component that exports a pin with single pin interface as interrupt.  I can watch it go high in an ILA for a single clock cycle when I want the interrupt to run.

 

On the PS I have the following code:

#define INTC_DEVICE_ID XPAR_SCUGIC_0_DEVICE_ID
 
  ////#define XPS_FPGA0_INT_ID 61U from xparameters.h
#define INTC_DEVICE_INT_ID XPS_FPGA0_INT_ID
 
  Status = XScuGic_Connect(&InterruptController, INTC_DEVICE_INT_ID,
                                                   (Xil_ExceptionHandler)DeviceDriverHandler,
                                                   (void *)&InterruptController);
   
  // If I simulate the interrupt without pulling the interrupt pin high it seems to work
 
   Status = XScuGic_SoftwareIntr(&InterruptController,
 
                                                           INTC_DEVICE_INT_ID,
 
                                                           XSCUGIC_SPI_CPU0_MASK);
 
    
 
   But it doesn't work with the real interrupt.  This is supposed to be easy, is there something I didn't do?  
 
   I can show all of the code, it is basically the example from he ScuGic example in the SDK.
 
    
 
   Thanks
  • Sign in to reply
  • Cancel
Parents
  • raymadigan
    0 raymadigan over 10 years ago

    I built a board with only the AXI Lite component that when a 1 is sent to register 0 it pulls an exported line high for one clock cycle.  The line is auto inferred to be an interrupt.  I can watch the line go high in an ILA.  Still the interrupt doesn't file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • raymadigan
    0 raymadigan over 10 years ago in reply to raymadigan

    I found the problem, Something I missed when I read the Speedway work twice, :(.  I wasn't setting the priority correct.  When I just used your values it worked in the isolated case and I suspect it will work in the product.  Thanks for all of your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago in reply to raymadigan

    Hi Raymadigan,

    Glad to hear! I appreciate you posting your solution as well. Hopefully it will help someone else in the future.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 10 years ago in reply to raymadigan

    Hi Raymadigan,

    Glad to hear! I appreciate you posting your solution as well. Hopefully it will help someone else in the future.

    --Josh