Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Custom Peripheral W/ Slave Interface
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 280 views
  • Users 0 members are here
Related

Custom Peripheral W/ Slave Interface

e14 Contributor
e14 Contributor over 12 years ago

Is it possible to create a custom peripheral with a slave interface so that I can connect it to a master interface on the axi interconnect?

If so, I was wondering what the structure of the code has to be in vhdl in order to create the slave interface.

Thanks,

Zach

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Lab 7 of the tutorial with the Avnet "Developing Zynq 7000 All Programmable SoC Hardware" Speedway Workshop steps you though how to create a custom peripheral with a slave axi interface and integrate it into your Zynq system. There are versions of the tutorial for both the ZedBoard and the MicroZed board. You can download the presentation material and labs here: http://www.zedboard.org/support/trainings-and-videos

     

    The lab example is implemented using Verilog but you could choose VHDL and implement in a similar fashion.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Lab 7 of the tutorial with the Avnet "Developing Zynq 7000 All Programmable SoC Hardware" Speedway Workshop steps you though how to create a custom peripheral with a slave axi interface and integrate it into your Zynq system. There are versions of the tutorial for both the ZedBoard and the MicroZed board. You can download the presentation material and labs here: http://www.zedboard.org/support/trainings-and-videos

     

    The lab example is implemented using Verilog but you could choose VHDL and implement in a similar fashion.

     

    -Gary