Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed Carrier Card IO
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 456 views
  • Users 0 members are here
Related

MicroZed Carrier Card IO

100pianoman
100pianoman over 8 years ago

Hello,

 
  
   
    

 I have a MicroZed SoC and a carrier card. I am trying to program a simple phase accumulator in Verilog (using Xilinx Vivado 2018.1), assign the variables to the contraint file through the "elaborated design" and IO planning, and load the bitstream onto the FPGA. I know that the 100 IOs on the microheader are unavailable unless you connect them to the carrier card. I have done so.
      I am using a 5V wall adapter to power the carrier card. I have the jumpers on the carrier card set to 1.8 V (same voltage as the IOSTANDARD in the constraint file), and the jumpers on the microzed are set to JTAG mode. I am able to load the bitstream successfully onto the microZed when the microzed is powered through the carrier board, and the microzed is attached to the JTAG programming port (J3); however, I am unable to get any voltage reading from the corresponding pins on the carrier card.
     
      Any help would be appreciated.
      Thanks,
      Matthew

   
  
 
  • Sign in to reply
  • Cancel
  • 100pianoman
    0 100pianoman over 8 years ago

    Hello,

    I figured out my problem. The pins on the JX1 and JX2 microheaders do not correspond to the CON1 and CON2 pins on the breakout carrier card. I looked in the hardware information for the breakout carrier board and found the answer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer