Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed Vivado Design Issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 362 subscribers
  • Views 1511 views
  • Users 0 members are here
Related

MicroZed Vivado Design Issue

raymadigan
raymadigan over 10 years ago

I am not sure what to do at this point.  I  have tried everything I can think of except a new MicroZed board.

I have a design that uses a custom AXI Lite IP.   Basically I want to allocate N registers and have N/2 be read/write and the other N/2 be read only.  The read only registers will be written to by my application. 

I have build the design and none of my changes have any effect when I run the application on my uZed.  I have commented out the entire process that writes the register to the AXI output pins.  This change has no effect on the application, it still runs as the original AXI Lite IP.

I have asked countless times in the Vivado, Design Entry, Zynq forums and nobody has an idea of how to overcome this problem.

I have a very very early uZed.  Is there any suggestions to overcome this issue.

Is there a test I can run to determine where the issue might be.

I have a very similar problem with an AXI Stream Master IP I am trying to build.

  • Sign in to reply
  • Cancel
Parents
  • raymadigan
    0 raymadigan over 10 years ago

    I looked closely at the vhdl to try to get a better understanding and saw this:

    tprocess (S_AXI_ACLK)
    tvariable loc_addr :std_logic_vector(OPT_MEM_ADDR_BITS downto 0);
    tbegin
    t  if rising_edge(S_AXI_ACLK) then
    t    if S_AXI_ARESETN = '0' then
    t      slv_reg0 <= (others => '0');
    t      slv_reg1 <= (others => '0');
    t      slv_reg2 <= (others => '0');
    t      slv_reg3 <= (others => '0');

    so all registers should be reset to zero when AXI_ARESETN goes to zero.

    int main()
    {
        init_platform();
        print("Hello World
    r");

        volatile int BaseAddress = 0x43C00000;

        // Check the initial state of the 0'th register
        int foo = CCMDEMO_mReadReg(&BaseAddress, 0);
        printf("Reg 0: %d
    r", foo);

        // Set the 0'th register to a value and read it
        CCMLITEDEMO_mWriteReg(&BaseAddress, 0, 54321);
        int bar = CCMLITEDEMO_mReadReg(&BaseAddress, 0);
        printf("Reg 0: %d
    r", bar);

        cleanup_platform();
        return 0;
    }

    shows output:

    Hello World
    Reg 0: 1136656384
    Reg 0: 54321

    It seems like it works, but maybe the reset is wrong.



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • raymadigan
    0 raymadigan over 10 years ago

    I looked closely at the vhdl to try to get a better understanding and saw this:

    tprocess (S_AXI_ACLK)
    tvariable loc_addr :std_logic_vector(OPT_MEM_ADDR_BITS downto 0);
    tbegin
    t  if rising_edge(S_AXI_ACLK) then
    t    if S_AXI_ARESETN = '0' then
    t      slv_reg0 <= (others => '0');
    t      slv_reg1 <= (others => '0');
    t      slv_reg2 <= (others => '0');
    t      slv_reg3 <= (others => '0');

    so all registers should be reset to zero when AXI_ARESETN goes to zero.

    int main()
    {
        init_platform();
        print("Hello World
    r");

        volatile int BaseAddress = 0x43C00000;

        // Check the initial state of the 0'th register
        int foo = CCMDEMO_mReadReg(&BaseAddress, 0);
        printf("Reg 0: %d
    r", foo);

        // Set the 0'th register to a value and read it
        CCMLITEDEMO_mWriteReg(&BaseAddress, 0, 54321);
        int bar = CCMLITEDEMO_mReadReg(&BaseAddress, 0);
        printf("Reg 0: %d
    r", bar);

        cleanup_platform();
        return 0;
    }

    shows output:

    Hello World
    Reg 0: 1136656384
    Reg 0: 54321

    It seems like it works, but maybe the reset is wrong.