Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Modifying MicroZed for USB Device Interface
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 643 views
  • Users 0 members are here
Related

Modifying MicroZed for USB Device Interface

e14 Contributor
e14 Contributor over 12 years ago

I would like to use the MicroZed as a USB Device (not Host). What hardware modifications are needed to do this? Are there any HID USB drivers that would run on a bare metal platform?

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 12 years ago

    Hi pschur,

    The modifications required are covered on Sheet 5 of the Rev. F schematic.  These changes are also covered in the MicroZed HW User Guide.

    MicroZed USB PHY is preconfigured for Host Mode operation by default.  The USB PHY can be configured for Device Mode operation through a set of hardware component population options.

    To modify MicroZed for operation in USB Device Mode, perform the following hardware changes:

    u2022tReplace R56 with 10K Ohm resistor
    u2022tRemove R50
    u2022tRemove L10 (Not populated by default)
    u2022tRemove C1 (Optional)
    u2022tRemove C3 (Optional)

    There is also an example posted in the MicroZed Reference Designs/Tutorial section which gives a SW example turning MicroZed into a small USB Mass Storage device.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jothin
    0 jothin over 11 years ago

    Hi
    I did the modifications explained in the guide. But the host did not detect zynq usb. I do not see any example of usb mass storage under reference_design/tutoril section. Please can you let know if anybody got this working

    Jothi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi,

    FYI: I made the changes to my MicroZed board as stated in the first post and had no trouble getting the board to work in device mode. Perhaps you should review your changes just to confirm.

    I've recently evaluated the mass storage device example on the MicroZed and everything worked well. See reference: http://zedboard.org/content/ise-146-version-1

    I hope this helps!
    Ed