Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design How to assign Clock pin in UCF file in Xilinx ISE project?- HELP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 562 views
  • Users 0 members are here
Related

How to assign Clock pin in UCF file in Xilinx ISE project?- HELP

e14 Contributor
e14 Contributor over 11 years ago

Hello,

I have made an I2S bus for MicroZed board to communicate with CODEC. I made the project in Xilinx ISE but could not find the system clock pin. I know the clock is available in PS, but how to assign it if I am not using PS and want to work with Xilinx ISE. Any solution?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi NaveedAnwar,

    Which MicroZed carrier are you using to prototype your design?

    In order to use clocks provided from the PS, you will need to run the ps7_init.tcl file or run a piece of software that executes the ps7_init.c functions to get the processing system PLLs up and running to the desired frequency.  I don't know if there is a way to do this directly from ISE without using SDK to configure the processing system.

    Alternatively, if you are using the MicroZed IO Carrier there is a 100MHz oscillator at X1 on the carrier board that is connected to a SRCC pin at K17 that you could use if you simply need a clock source.

    That oscillator will also need to be enabled by pulling pin K18 high.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi NaveedAnwar,

    Which MicroZed carrier are you using to prototype your design?

    In order to use clocks provided from the PS, you will need to run the ps7_init.tcl file or run a piece of software that executes the ps7_init.c functions to get the processing system PLLs up and running to the desired frequency.  I don't know if there is a way to do this directly from ISE without using SDK to configure the processing system.

    Alternatively, if you are using the MicroZed IO Carrier there is a 100MHz oscillator at X1 on the carrier board that is connected to a SRCC pin at K17 that you could use if you simply need a clock source.

    That oscillator will also need to be enabled by pulling pin K18 high.

    Regards,

    -Kevin