Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed doesn't start up
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 28 replies
  • Subscribers 362 subscribers
  • Views 4132 views
  • Users 0 members are here
Related

MicroZed doesn't start up

vatsalnaik
vatsalnaik over 9 years ago

I have MicroZed Industrial grade. There are no jumpers JP1, JP2, JP3. So I cannot boot it from SD card. 

I don't see anything on the COM port. I can only Program FPGA but when I try to run simple Hello World - Launch on Hardware, it gives me these errors

An internal error occurred during: "Launching System Debugger on Local hello1.elf".
No Active System

ERROR : fpga initialization failed

Error while launching program: 
AP transaction error, DAP status f0000021
 
 

When programming with QSPI, following was the error:

 
Cannot access DDR: the controller is held in reset
 
at com.xilinx.sdk.targetmanager.internal.TM.downloadELF(TM.java:686)
at com.xilinx.sdk.debug.core.internal.AppRunner.run(AppRunner.java:129)
at com.xilinx.sdk.debug.core.XilinxAppLaunchConfigurationDelegate.runApplication(XilinxAppLaunchConfigurationDelegate.java:637)
at com.xilinx.sdk.debug.core.XilinxAppLaunchConfigurationDelegate.launch(XilinxAppLaunchConfigurationDelegate.java:309)
at com.xilinx.sdk.debug.ui.XilinxAppLaunchDelegateWrapper.launch(XilinxAppLaunchDelegateWrapper.java:31)
 
 
What should I do? Thank you.
  • Sign in to reply
  • Cancel
Parents
  • vatsalnaik
    0 vatsalnaik over 9 years ago

    The way I received board is, jumpers are in default connection to boot from QSPI. There is no way I can change its boot configuration, that's why I am not able to load a uBOOT file to SD card and boot it from there. 

    If you want to give me an email I will send the picture of the board. I won't able to upload pics here. Don't know how it passed quality control. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vatsalnaik
    0 vatsalnaik over 9 years ago

    The way I received board is, jumpers are in default connection to boot from QSPI. There is no way I can change its boot configuration, that's why I am not able to load a uBOOT file to SD card and boot it from there. 

    If you want to give me an email I will send the picture of the board. I won't able to upload pics here. Don't know how it passed quality control.