Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Negative Timing Slack using MicroZed Board Defintion File in Vivado 2017.1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 364 subscribers
  • Views 2607 views
  • Users 0 members are here
Related

Negative Timing Slack using MicroZed Board Defintion File in Vivado 2017.1

e14 Contributor
e14 Contributor over 9 years ago

When upgrading to Vivado 2017.1, using the Microzed Board definition file for 2016.4 I get an critical warning on the ddr interface.

The critical warning is:

PCW_UI_PARAM_DDR_DQS_TO_CLK_DELAY_0 has negative value -0.073. PS_DDR interfaces might fail when entering negative DQS skew values.

There is also a warning on DELAY_1 -0.072.

These critical warnings result in negative timing slack.

Any suggestions on what should to do about this error. I'm tempted to ignore it, but I don't want to miss any timing issues I might create in my code.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I was able to recreate the problem again.

    First I created a system in Vivado 2015.2 with a PS and block automation to connect up the DDR, just like in my above comment. I built this system no problem. I used the 2015.1 Board definition file for the microzed (v1.0 vs v1.1).

    Then I opened the same project in Vivado 2017.1. It asked if I wanted to automatically upgrade the project, I said yes. It then said that my IP was out of date and wanted me to update the PS to the latest version. I updated it in the IP status tab to the latest version. During the upgrade of the PS IP, I recieved the critical warnings above. I also got a message saying the board_part definition of 1.0 was not found (which I know its not there, I only have 1.1 installed for 2017.1) - Which leads me to believe the 1.1 board preset file is fine and there is something going on behind the scenes causing the error.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I was able to recreate the problem again.

    First I created a system in Vivado 2015.2 with a PS and block automation to connect up the DDR, just like in my above comment. I built this system no problem. I used the 2015.1 Board definition file for the microzed (v1.0 vs v1.1).

    Then I opened the same project in Vivado 2017.1. It asked if I wanted to automatically upgrade the project, I said yes. It then said that my IP was out of date and wanted me to update the PS to the latest version. I updated it in the IP status tab to the latest version. During the upgrade of the PS IP, I recieved the critical warnings above. I also got a message saying the board_part definition of 1.0 was not found (which I know its not there, I only have 1.1 installed for 2017.1) - Which leads me to believe the 1.1 board preset file is fine and there is something going on behind the scenes causing the error.