Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Petalinux 2020.1 build for MicroZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 360 subscribers
  • Views 1042 views
  • Users 0 members are here
Related

Petalinux 2020.1 build for MicroZed

ldeevans
ldeevans over 5 years ago

Hi,

I'm still trying to build an image for the microzed 7010:

I followed instructions from here: Using Avnet Build Scripts to Build a PetaLinux BSP (2019.2 and earlier) , thank you narrucmot for the info. as well as UG1144.

The steps I think I need to do are:

 

To Build the 2020.1 BSP:

cd ~

mkdir -p git/avnet

cd git/avnet

git clone git://github.com/avnet/bdf.git -b master

git clone git://github.com/avnet/hdl.git -b 2020.1

git clone git://github.com/avnet/petalinux.git -b 2020.1

 

cd /home/stanley/git/avnet/petalinux/scripts

source /tools/Xilinx/Vivado/2020.1/settings64.sh

source ~/petalinux/settings.sh

vi /tools/Xilinx/Vivado/2020.1/bin/vivado # add "ulimit -s 16384"

./make_mz7010_fmccc.sh

 

Build a new project from the BSP:

cd ~/projects/petalinux

petalinux-create -t project -s ~/git/avnet/petalinux/projects/mz7010_fmccc_2020_1.bsp

cd mz7010_fmccc_2020_1/

petalinux-config --get-hw-description=~/git/avnet/hdl/Projects/mz_petalinux/MZ7010_FMCCC_2020_1 # for MZ7010_FMCCC.xsa

petalinux-config -c rootfs

petalinux-config -c kernel

petalinux-build

 

I eventually get the following error:

INFO: sourcing build tools

[INFO] building petalinux-image-minimal

[INFO] sourcing build environment

[INFO] generating user layers

[INFO] generating workspace directory

INFO: bitbake petalinux-image-minimal

Loading cache: 100% |################################################################################################################################| Time: 0:00:01

Loaded 4259 entries from dependency cache.

Parsing recipes: 100% |##############################################################################################################################| Time: 0:02:03

Parsing of 2992 .bb files complete (2990 cached, 2 parsed). 4261 targets, 198 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

Initialising tasks: 100% |###########################################################################################################################| Time: 0:00:02

Checking sstate mirror object availability: 100% |###################################################################################################| Time: 0:00:10

Sstate summary: Wanted 125 Found 16 Missed 109 Current 880 (12% match, 89% complete)

NOTE: Executing Tasks

NOTE: Setscene tasks completed

ERROR: petalinux-image-minimal-1.0-r0 do_image_wic: No kickstart files from WKS_FILES were found: petalinux-image-minimal.mz7010-fmccc.wks petalinux-image-minimal.wks. Please set WKS_FILE or WKS_FILES appropriately.

ERROR: petalinux-image-minimal-1.0-r0 do_image_wic: Execution of '/home/stanley/projects/petalinux/mz7010_fmccc_2020_1/build/tmp/work/mz7010_fmccc-xilinx-linux-gnueabi/petalinux-image-minimal/1.0-r0/temp/run.do_image_wic.22626' failed with exit code 1:

WARNING: /home/stanley/projects/petalinux/mz7010_fmccc_2020_1/build/tmp/work/mz7010_fmccc-xilinx-linux-gnueabi/petalinux-image-minimal/1.0-r0/temp/run.do_image_wic.22626:1 exit 1 from 'exit 1'

ERROR: Logfile of failure stored in: /home/stanley/projects/petalinux/mz7010_fmccc_2020_1/build/tmp/work/mz7010_fmccc-xilinx-linux-gnueabi/petalinux-image-minimal/1.0-r0/temp/log.do_image_wic.22626

ERROR: Task (/home/stanley/projects/petalinux/mz7010_fmccc_2020_1/components/yocto/layers/meta-petalinux/recipes-core/images/petalinux-image-minimal.bb:do_image_wic) failed with exit code '1'

NOTE: Tasks Summary: Attempted 3653 tasks of which 3652 didn't need to be rerun and 1 failed.

Summary: 1 task failed:

  /home/stanley/projects/petalinux/mz7010_fmccc_2020_1/components/yocto/layers/meta-petalinux/recipes-core/images/petalinux-image-minimal.bb:do_image_wic

Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

ERROR: Failed to build petalinux-image-minimal

 

There are .wic files available such as avnet-image-minimal-mz7010-fmccc.wic and rootfs.wic, do I need to generate this ?

 

Also, it is not clear to me if building petalinux-image-minimal will include any apps created with:

petalinux-create -t apps --template c --name myapp --enable ?

 

Building avnet-image-minimal does build OK, but does not include myapp, am I on the right path please?

 

Kind Regards, Dave.