Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed 7010- trace delay max//min
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 1652 views
  • Users 0 members are here
Related

Microzed 7010- trace delay max//min

RAJAT99
RAJAT99 over 3 years ago

Hello, I am using microzed 7010. I have to set trace delay max/min in constraints input for data coming from ADC. How to calculate these parameters?

imageimage

  • Sign in to reply
  • Cancel

Top Replies

  • flyingbean
    flyingbean over 3 years ago +1
    Xilinx has some training material on this topic: https://xilinx.github.io/xup_fpga_vivado_flow/lab5.html The basic idea on the input delay analysis is to give us timing budget on FPGA/board level…
  • flyingbean
    flyingbean over 3 years ago in reply to RAJAT99 +1
    Trce_dly_min/mac can use an estimated placeholder such as +-2.5% of the clock speed, which is normally used for high speed signal board level layout design. I assumed that MicroZed board layout followed…
Parents
  • flyingbean
    flyingbean over 3 years ago

    Xilinx has some training material on this topic:

    https://xilinx.github.io/xup_fpga_vivado_flow/lab5.html

    image

    The basic idea on the input delay analysis is to give us timing budget on FPGA/board level design. Tco is related to the clock speed. Put a number there to define the clock uncertain range. trce_dly_min/max should be from the PCB layout file.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • flyingbean
    flyingbean over 3 years ago

    Xilinx has some training material on this topic:

    https://xilinx.github.io/xup_fpga_vivado_flow/lab5.html

    image

    The basic idea on the input delay analysis is to give us timing budget on FPGA/board level design. Tco is related to the clock speed. Put a number there to define the clock uncertain range. trce_dly_min/max should be from the PCB layout file.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • RAJAT99
    RAJAT99 over 3 years ago in reply to flyingbean

    Thanks flyingbean . I am using microzed 7z010 board. Trce_dly_min/max will be calculated from microzed 7z010 board layout file? If yes then how to calculate?

    I have go through training material. How tco and trce_dly_min/max for input and output delay constraint selected(not explained in it)?  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • flyingbean
    flyingbean over 3 years ago in reply to RAJAT99

    Trce_dly_min/mac can use an estimated placeholder such as +-2.5% of the clock speed, which is normally used for high speed signal board level layout design. I assumed that MicroZed  board layout followed such design constraint. Here is the board layout net length data from Avnet website: www.avnet.com/.../

    image

    You might need to convert the physical trace length into trace time/latency. Rule of thrum of trace length to time: 15~17cm/ns. (https://support.xilinx.com/s/question/0D52E00006hplPcSAI/what-do-trcedlymax-and-trcedlymin-mean-when-setting-output-delay-constraints?language=ja)

    FPGA timing constraints explanation can be found from this support ticket;

    https://support.xilinx.com/s/article/63174?language=en_US

    Which is similar way I used for this topic.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • RAJAT99
    RAJAT99 over 3 years ago in reply to flyingbean

    Thanks flyingbean