Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design How to red DDR vs BRAM
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 331 subscribers
  • Views 1346 views
  • Users 0 members are here
Related

How to red DDR vs BRAM

quadzilla
quadzilla over 1 year ago

This is another doubtlessly naive question.  I know that you can read the BRAM by using XBram_ReadReg() and a BRAM controller.  Also that XBram_ReadReg() basically amounts to using Xil_In32() to read a memory location.

Can we do something similar to read the DDR RAM, or are we always forced to use the routines in xaxidma_bdring.c?

  • Sign in to reply
  • Cancel

Top Replies

  • viktornikolov
    viktornikolov over 1 year ago +1
    You connect DDR SDRAM using MIG IP (Memory Interface Generator). MIG connects to AXI Interconnect and then you use it as a memory by the code running on the CPU. See this tutorial I created for using…
  • viktornikolov
    0 viktornikolov over 1 year ago

    You connect DDR SDRAM using MIG IP (Memory Interface Generator). MIG connects to AXI Interconnect and then you use it as a memory by the code running on the CPU.

    See this tutorial I created for using DDR SDRAM with the MicroBlaze Soft CPU. The tutorial uses a Digilent development board, nevertheless, most of the steps are applicable to any other Xilinx FPGA board.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • quadzilla
    0 quadzilla over 1 year ago in reply to viktornikolov

    Many thanks. I will step through it now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • youngn111
    0 youngn111 over 1 year ago

    Once you have the DDR connected to the CPU via AXI Interconnect, it will be memory-mapped into the CPU's address space.

    You can then use a Xil_In32() call to get the data, or you could dereference a pointer as follows:

    // Declare a pointer with memory location 0x3000_0000, and declare an u32 to hold data

    unsigned int *punData;

    unsigned int unData;

    // Get the data at the location held by the pointer

    unData = *punData;

    unData would then contain the data from address 0x30000000

    Be aware that data in the DDR is cached.  If you are accessing DDR memory that was (only) loaded by the CPU, then it will read back correctly.

    If you are accessing data that was loaded by the PL, then you probably have to invalidate the CPU's cache before reading it to ensure you get the data loaded by the CPU, and not stale data leftover in the CPU cache.

    It looks like you are using a bare metal application, so to accomplish this, take a look at the following functions:

    void Xil_DCacheInvalidate(void);
    void Xil_DCacheInvalidateRange(INTPTR adr, u32 len);
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • quadzilla
    0 quadzilla over 1 year ago in reply to youngn111

    Thanks for the tip, and I will try it out.  I couldn't find 0x3000000 listed anywhere in xparameters.h though.  Where did you find this documented?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • viktornikolov
    0 viktornikolov over 1 year ago in reply to quadzilla

    If you use MIG in the HW design, the lscript.ld in Vitis will show address and size of DDR memory (and any other available memories).

    image

    Corresponding macros are also generated in xparameters.h

    /* Definitions for peripheral MIG_7SERIES_0 */
    #define XPAR_MIG_7SERIES_0_BASEADDR 0x80000000
    #define XPAR_MIG_7SERIES_0_HIGHADDR 0x8FFFFFFF

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • quadzilla
    0 quadzilla over 1 year ago in reply to viktornikolov

    Thanks for the tip.  Looks like the proper address is 0x80000000 rather than 0x30000000 though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • padudle
    0 padudle over 1 year ago

    If you are using DDR memory you are probably accessing large blocks of data.  Directly accessing the MIG DDR using pointers, etc will result in one transfer per call.  DDR, AXI and the MIG are designed to provide efficient bursts of contiguous address locations. The only way I have found to get efficient DDR access by using the DMA logic.  If you are running Linux on a Zynq you can use the xilinx xdma (or is it zdma?) to move data in and out of the DDR.