Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed Board Definition File (BDF) DDR Settings
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 657 views
  • Users 0 members are here
Related

Microzed Board Definition File (BDF) DDR Settings

padudle
padudle over 1 year ago

Hello,

I am trying to use a Microzed board to demonstrate some ideas using the latest Vivado 2024.2 and Avnet-Tria BDF files.  Unfortunately, I have not been able to get the DDR3 memory to run reliably.

First, I tried to boot Petalinux but operation was erratic. In most cases the board did not send any text to the console after pressing the reset button.  I suspected the DDR3 memory so I built a Vitis bare metal application but I also found it to be very unreliable running from the DDR3 which is the default.  Finally, I edited the linker script to put .data, .text and .bss in the Zynq On-Chip Memory (OCM).  This boots and runs reliably.

Next, I looked at the DDR3 settings in the IP Integrator block diagram of my FPGA design.  At a glance I can see that the memory size is not set correctly.  The settings call out 2048Mb per chip while the chips are actually 256Mx16 = 4096Mb.  In my Vitis project I can see it thinks the DDR3 is only 512MB in size.  I have looked a the Microzed schematics, Rev H and Rev F, and they both have 1GB DDR3.

The DDR3 settings in my FPGA project come from the Avnet BDF file for the Microblaze.  I am using https://github.com/Avnet/bdf/tree/master/microzed_7020/1.4. 

I think this means there are errors in the Microblaze BDF that prevent correct operation.

  • Sign in to reply
  • Cancel
  • padudle
    padudle over 1 year ago

    I'm not sure how it happened but the DDR part type was set wrong in my project. Anyway, here is the change in my TCL script that creates the block diagram and now my Vitis app runs fine in DDR.

    -    CONFIG.PCW_UIPARAM_DDR_PARTNO {MT41J128M16 HA-15E} \
    +    CONFIG.PCW_UIPARAM_DDR_PARTNO {MT41K256M16 RE-125} \

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • padudle
    padudle over 1 year ago

    I see how I got those wrong DDR settings.  I carried that IPI design from an old ZedBoard project that has only 512MB DDR3 and the MT41J part.