Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed Board Definition File (BDF) DDR Settings
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 657 views
  • Users 0 members are here
Related

Microzed Board Definition File (BDF) DDR Settings

padudle
padudle over 1 year ago

Hello,

I am trying to use a Microzed board to demonstrate some ideas using the latest Vivado 2024.2 and Avnet-Tria BDF files.  Unfortunately, I have not been able to get the DDR3 memory to run reliably.

First, I tried to boot Petalinux but operation was erratic. In most cases the board did not send any text to the console after pressing the reset button.  I suspected the DDR3 memory so I built a Vitis bare metal application but I also found it to be very unreliable running from the DDR3 which is the default.  Finally, I edited the linker script to put .data, .text and .bss in the Zynq On-Chip Memory (OCM).  This boots and runs reliably.

Next, I looked at the DDR3 settings in the IP Integrator block diagram of my FPGA design.  At a glance I can see that the memory size is not set correctly.  The settings call out 2048Mb per chip while the chips are actually 256Mx16 = 4096Mb.  In my Vitis project I can see it thinks the DDR3 is only 512MB in size.  I have looked a the Microzed schematics, Rev H and Rev F, and they both have 1GB DDR3.

The DDR3 settings in my FPGA project come from the Avnet BDF file for the Microblaze.  I am using https://github.com/Avnet/bdf/tree/master/microzed_7020/1.4. 

I think this means there are errors in the Microblaze BDF that prevent correct operation.

  • Sign in to reply
  • Cancel
Parents
  • padudle
    padudle over 1 year ago

    I see how I got those wrong DDR settings.  I carried that IPI design from an old ZedBoard project that has only 512MB DDR3 and the MT41J part.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • padudle
    padudle over 1 year ago

    I see how I got those wrong DDR settings.  I carried that IPI design from an old ZedBoard project that has only 512MB DDR3 and the MT41J part.