Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design fpga programming using Ubuntu 18.04
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 355 subscribers
  • Views 1831 views
  • Users 0 members are here
  • mini-itx_hardware_design
Related

fpga programming using Ubuntu 18.04

amamory
amamory over 6 years ago

Hello,

 

I am testing a mini-itx board with Ubuntu 18.04 host OS.

 

The tests with builtin software went ok. However, when i try to program the FPGA via this module

https://store.digilentinc.com/jtag-smt2-surface-mount-programming-module/

 

The USB device is not even recognized. I checked with 'dmesg' command. Nothing changes when i plug the usb in or out.

 

It seems that there are 2 possibilities:

1) there is a special device driver for https://store.digilentinc.com/jtag-smt2-surface-mount-programming-module/

2) there is some jumper to allow jtag programming that I am missing.

 

Reading the manual, I see that SW7[1] enables the JTAG Cascaded. I switched this on and off and nothing changes. The USB port is not recognized.

 

So, what is necessary to have the USB JTAG working on Linux ?

 

best regards,

Alexandre

  • Sign in to reply
  • Cancel
  • amamory
    amamory over 6 years ago

    I just want to add that I have other boards, such as zedboard, and I can program them without problems. The issue I described earlier is related only with mini-itx board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cybero
    cybero over 6 years ago

    did you find the solution to this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bhfletcher
    bhfletcher over 5 years ago in reply to cybero

    We have seen SMT2 failures before. Does anything in this thread sound familiar? You could likely solve the problem by replacing the SMT2.

    Cannot detect Ultrazed Board on host PC using UART and JTAG.

     

    https://www.newark.com/digilent/410-251-b/jtag-smt2-baked-msl3/dp/51AH5649

     

     

    Bryan